JointmarkPointsBuilderPointPosition Enumeration¶
NXOpen.Weld.JointmarkPointsBuilder.PointPosition is an alias for NXOpen.Weld.JointmarkPointsBuilderPointPosition
-
class
NXOpen.Weld.
JointmarkPointsBuilderPointPosition
¶ Bases:
object
The point classification
Enum Members
Enum Member Enum Member Description NotSet None specifed.MovedAlongGuide User moved point from default location along the guide curveMovedOffGuide User moved point from default location off the guide curve-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-