WeldObjectBuilderCommandName Enumeration¶
NXOpen.Weld.WeldObjectBuilder.CommandName is an alias for NXOpen.Weld.WeldObjectBuilderCommandName
-
class
NXOpen.Weld.
WeldObjectBuilderCommandName
¶ Bases:
object
Commands that a callback will be invoked after dialog completion.
Enum Members
Enum Member Enum Member Description NotSet No command. Used to initialize value.Groove Groove Weld commandFillet Fillet Weld commandUserDefined User Defined Weld commandWeldPoint Weld Point commandBead Bead commandFill Fill commandImportCsv Import CSV commandEasySpot Easy Spot commandDatumLocator Datum Locator commandMeasurementLocator Measurement Locator commandEasyMeasurementPattern Easy Measurement Pattern commandPlugSlot Plug Slot commandJoint Welding Joint commandDatumSurface Datum Surface commandDatumPin Datum Pin commandSurfaceWeld Surface Weld commandCompound Compound Weld commandWeldAttribute Edit Weld AttributeJointDefinition Edit Joint Definition ParametersJointmark Joint Mark commandWeldPointWizard Weld Point Wizard command-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-