WeldGrooveType Enumeration

class NXOpen.Weld.WeldGrooveType

Bases: object

Groove Creation Type Enum Members

Enum Member Enum Member Description
EdgesNotPrepared
Edges are not prepared
EdgesPrepared
Edges are prepared
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.