DatumCommonBuilderControlMethodTypes Enumeration¶
NXOpen.Weld.DatumCommonBuilder.ControlMethodTypes is an alias for NXOpen.Weld.DatumCommonBuilderControlMethodTypes
-
class
NXOpen.Weld.
DatumCommonBuilderControlMethodTypes
¶ Bases:
object
Settings for the method used to define the control direction.
Enum Members
Enum Member Enum Member Description PrincipalAxis A principal axis. Absolute X,Y, or ZUseSectionPlane Not a principal axis, use Section Plane-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-