WeldGrooveBuilderTypes Enumeration¶
NXOpen.Weld.WeldGrooveBuilder.Types is an alias for NXOpen.Weld.WeldGrooveBuilderTypes
-
class
NXOpen.Weld.
WeldGrooveBuilderTypes
¶ Bases:
object
The types of Groove to create
Enum Members
Enum Member Enum Member Description SquareButt Square ButtVGroove V GrooveBevelGroove Bevel GrooveUGroove U GrooveJGroove J GrooveFlaredVGroove Flared V GrooveFlaredBevelGroove Flared Bevel GrooveFillinFlaredVGroove FillinFlaredBevelGroove Fillin Flared Bevel Groove-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-