WeldBeadPathBuilderOffsetMethodType Enumeration

NXOpen.Weld.WeldBeadPathBuilder.OffsetMethodType is an alias for NXOpen.Weld.WeldBeadPathBuilderOffsetMethodType

class NXOpen.Weld.WeldBeadPathBuilderOffsetMethodType

Bases: object

Settings to indicate the desired offset method.

Enum Members

Enum Member Enum Member Description
InFace
offset in selected primary faces
Centerline
centerline of overlapping sheets
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.