WeldPointExitBuilder Class¶
-
class
NXOpen.Weld.
WeldPointExitBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.Weld.WeldPointExitBuilder
class used to pass welding object from the Weld Point command to a user callback.This object is not used on edit. .. versionadded:: NX8.0.2
Properties¶
Property | Description |
---|---|
CommandUsed | Returns the command name that was last used to create features. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
GetFeatureInformation | Gets the information for the newly created features. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
WeldPointExitBuilderCommandName Enumeration | The command name used for the newly created features. |
WeldPointExitBuilderMethodUsed Enumeration | The method use to create the features. |
Structs¶
WeldPointExitBuilderFeatureInfo_Struct Struct |
|
Property Detail¶
CommandUsed¶
-
WeldPointExitBuilder.
CommandUsed
¶ Returns the command name that was last used to create features.
This callback is not called on edit.
-------------------------------------
Getter Method
Signature
CommandUsed()
Returns: command name used Return type: NXOpen.Weld.WeldPointExitBuilderCommandName
New in version NX8.0.2.
License requirements: None.
Method Detail¶
GetFeatureInformation¶
-
WeldPointExitBuilder.
GetFeatureInformation
¶ Gets the information for the newly created features.
Signature
GetFeatureInformation()
Returns: features created Return type: list of NXOpen.Weld.WeldPointExitBuilderFeatureInfo_Struct
New in version NX8.0.2.
License requirements: None.
Validate¶
-
WeldPointExitBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.