WeldPointExitBuilderCommandName Enumeration¶
NXOpen.Weld.WeldPointExitBuilder.CommandName is an alias for NXOpen.Weld.WeldPointExitBuilderCommandName
-
class
NXOpen.Weld.
WeldPointExitBuilderCommandName
¶ Bases:
object
The command name used for the newly created features.
Enum Members
Enum Member Enum Member Description NotSet No command. Used to initialize value.WeldPoint Weld Point commandDatumLocator Datum Locator commandMeasurementLocator Measurement Locator commandJointmark Joint Mark commandWeldPointWizard Weld Point Wizard command-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-