WeldMeasurementSizeMethod Enumeration

class NXOpen.Weld.WeldMeasurementSizeMethod

Bases: object

the size method for measurement Enum Members

Enum Member Enum Member Description
Invalid
Invalid size method
Auto
auto size method
Manual
manual size method
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.