WeldFacesetIndex Enumeration

class NXOpen.Weld.WeldFacesetIndex

Bases: object

the index of user picked face sets Enum Members

Enum Member Enum Member Description
First
first face set
Second
second face set
Third
third face set
Forth
forth face set
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.