PointMarkBuilderWeldTypes Enumeration¶
NXOpen.Weld.PointMarkBuilder.WeldTypes is an alias for NXOpen.Weld.PointMarkBuilderWeldTypes
-
class
NXOpen.Weld.
PointMarkBuilderWeldTypes
¶ Bases:
object
The weld type to create.
Enum Members
Enum Member Enum Member Description ResistanceSpot Resistance SpotArcSpot Arc SpotClinch ClinchDollop DollopWeldNut Weld NutWeldStud Weld StudCustom1 Custom 1 as defined in customer defaultsCustom2 Custom 2 as defined in customer defaultsCustom3 Custom 3 as defined in customer defaultsCustom4 Custom 4 as defined in customer defaultsCustom5 Custom 5 as defined in customer defaults-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-