DatumCommonBuilderCreationDirectionMethods Enumeration

NXOpen.Weld.DatumCommonBuilder.CreationDirectionMethods is an alias for NXOpen.Weld.DatumCommonBuilderCreationDirectionMethods

class NXOpen.Weld.DatumCommonBuilderCreationDirectionMethods

Bases: object

Settings to define the creation direction.

Enum Members

Enum Member Enum Member Description
Default
Use the default construction method
Opposite
Reverse the construction orientation
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.