EasyPatternBuilderSpacingMethodTypes Enumeration

NXOpen.Weld.EasyPatternBuilder.SpacingMethodTypes is an alias for NXOpen.Weld.EasyPatternBuilderSpacingMethodTypes

class NXOpen.Weld.EasyPatternBuilderSpacingMethodTypes

Bases: object

Indicates whether planes should be cut a grid lines, or if a single plane should be used.

Enum Members

Enum Member Enum Member Description
Grid
Use Grid spacing to cut sections.
SinglePlane
Use a single plane to cut a sections.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.