DatumCommonBuilder Class

class NXOpen.Weld.DatumCommonBuilder

Bases: NXOpen.Builder

Used to create or edit a NXOpen.Weld.DatumSurface or NXOpen.Weld.DatumPin feature.

This is an abstract class and cannot be directly instantiated

New in version NX8.5.0.

Properties

Property Description
AdditionalReferences Returns the additional references.
Characteristics Returns the characteristics.
ControlMethod Returns or sets the control method.
CreateDirectionVector Returns or sets the option to control if a reference datum axis should be output with this feature.
CreatePlane Returns or sets the option to control if a reference datum plane should be output with the this feature.
CreatePoint Returns or sets the option to control if a reference point should be output with this feature.
CreationDirection Returns or sets the creation direction.
CustomAboveLength Returns or sets the length above the datum reference point.
CustomRadius Returns or sets the radius of the solid sphere, cylinder or cone created.
CustomTotalLength Returns or sets the total length of the cylinder or cone along the direction axis.
CustomType Returns or sets the custom datum type.
CustomTypeName Returns or sets the custom name used to create the datum.
Derived Returns or sets the indicator if this should be marked as a derived from another datum.
DirectionAxis Returns or sets the direction axis.
DirectionLength Returns or sets the length of the datum axis vector created.
ModelingTolerance Returns or sets the modeling distance tolerance.
PlaneHeight Returns or sets the plane height along the direction axis.
PlaneWidth Returns or sets the plane width perpendicular to the direction axis.
PrincipalAxisX Returns or sets the principal axis x.
PrincipalAxisY Returns or sets the principal axis y.
PrincipalAxisZ Returns or sets the principal axis z.
ProjectAlongDirection Returns or sets the project along direction.
SectionPlaneNormal Returns or sets the section plane normal.
SolidType Returns or sets the solid body type specified.
Tag Returns the Tag for this object.

Methods

Method Description
Commit Commits any edits that have been applied to the builder.
Destroy Deletes the builder, and cleans up any objects created by the builder.
GetCommittedObjects For builders that create more than one object, this method returns the objects that are created by commit.
GetObject Returns the object currently being edited by this builder.
ShowResults Updates the model to reflect the result of an edit to the model for all builders that support showing results.
UpdateWithDerivedDatum Initialize the builder with the inputs from an existing datum.
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Enumerations

DatumCommonBuilderControlMethodTypes Enumeration Settings for the method used to define the control direction.
DatumCommonBuilderCreationDirectionMethods Enumeration Settings to define the creation direction.
DatumCommonBuilderCustomTypes Enumeration The custom type of the datum specified for creation.
DatumCommonBuilderSolidTypes Enumeration Settings for defining the solid type to create for the datum object.

Property Detail

AdditionalReferences

DatumCommonBuilder.AdditionalReferences

Returns the additional references.

Use to define addtion parts the datum connects.

-------------------------------------

Getter Method

Signature AdditionalReferences()

Returns:
Return type:NXOpen.Assemblies.SelectComponentList

New in version NX8.5.0.

License requirements: None.

Characteristics

DatumCommonBuilder.Characteristics

Returns the characteristics.

Used to specify additional attributes.

-------------------------------------

Getter Method

Signature Characteristics()

Returns:
Return type:NXOpen.Weld.CharacteristicsBuilder

New in version NX8.5.0.

License requirements: None.

ControlMethod

DatumCommonBuilder.ControlMethod

Returns or sets the control method.

The method for fixing the datum orientation.

-------------------------------------

Getter Method

Signature ControlMethod()

Returns:
Return type:NXOpen.Weld.DatumCommonBuilderControlMethodTypes

New in version NX8.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature ControlMethod(controlMethod)

Parameters:controlMethod (NXOpen.Weld.DatumCommonBuilderControlMethodTypes) –

New in version NX8.5.0.

License requirements: ugweld (“UG WELD”)

CreateDirectionVector

DatumCommonBuilder.CreateDirectionVector

Returns or sets the option to control if a reference datum axis should be output with this feature.

-------------------------------------

Getter Method

Signature CreateDirectionVector()

Returns:
Return type:bool

New in version NX8.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature CreateDirectionVector(createDirectionVector)

Parameters:createDirectionVector (bool) –

New in version NX8.5.0.

License requirements: ugweld (“UG WELD”)

CreatePlane

DatumCommonBuilder.CreatePlane

Returns or sets the option to control if a reference datum plane should be output with the this feature.

-------------------------------------

Getter Method

Signature CreatePlane()

Returns:
Return type:bool

New in version NX8.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature CreatePlane(createPlane)

Parameters:createPlane (bool) –

New in version NX8.5.0.

License requirements: ugweld (“UG WELD”)

CreatePoint

DatumCommonBuilder.CreatePoint

Returns or sets the option to control if a reference point should be output with this feature.

-------------------------------------

Getter Method

Signature CreatePoint()

Returns:
Return type:bool

New in version NX8.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature CreatePoint(createPoint)

Parameters:createPoint (bool) –

New in version NX8.5.0.

License requirements: ugweld (“UG WELD”)

CreationDirection

DatumCommonBuilder.CreationDirection

Returns or sets the creation direction.

-------------------------------------

Getter Method

Signature CreationDirection()

Returns:
Return type:NXOpen.Weld.DatumCommonBuilderCreationDirectionMethods

New in version NX8.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature CreationDirection(creationDirection)

Parameters:creationDirection (NXOpen.Weld.DatumCommonBuilderCreationDirectionMethods) –

New in version NX8.5.0.

License requirements: ugweld (“UG WELD”)

CustomAboveLength

DatumCommonBuilder.CustomAboveLength

Returns or sets the length above the datum reference point.

This is used if a cylinder or cone are created.

-------------------------------------

Getter Method

Signature CustomAboveLength()

Returns:
Return type:float

New in version NX8.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature CustomAboveLength(directionLength)

Parameters:directionLength (float) –

New in version NX8.5.0.

License requirements: ugweld (“UG WELD”)

CustomRadius

DatumCommonBuilder.CustomRadius

Returns or sets the radius of the solid sphere, cylinder or cone created.

-------------------------------------

Getter Method

Signature CustomRadius()

Returns:
Return type:float

New in version NX8.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature CustomRadius(customRadius)

Parameters:customRadius (float) –

New in version NX8.5.0.

License requirements: ugweld (“UG WELD”)

CustomTotalLength

DatumCommonBuilder.CustomTotalLength

Returns or sets the total length of the cylinder or cone along the direction axis.

-------------------------------------

Getter Method

Signature CustomTotalLength()

Returns:
Return type:float

New in version NX8.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature CustomTotalLength(customTotalLength)

Parameters:customTotalLength (float) –

New in version NX8.5.0.

License requirements: ugweld (“UG WELD”)

CustomType

DatumCommonBuilder.CustomType

Returns or sets the custom datum type.

This cooresponds to an entry in the customer defaults.

-------------------------------------

Getter Method

Signature CustomType()

Returns:
Return type:NXOpen.Weld.DatumCommonBuilderCustomTypes

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature CustomType(customType)

Parameters:customType (NXOpen.Weld.DatumCommonBuilderCustomTypes) –

New in version NX9.0.0.

License requirements: ugweld (“UG WELD”)

CustomTypeName

DatumCommonBuilder.CustomTypeName

Returns or sets the custom name used to create the datum.

-------------------------------------

Getter Method

Signature CustomTypeName()

Returns:Name of custom data type used from customer defaults
Return type:str

New in version NX8.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature CustomTypeName(customTypeName)

Parameters:customTypeName (str) – Custom datum type from customer defaults to use

New in version NX8.5.0.

License requirements: ugweld (“UG WELD”)

Derived

DatumCommonBuilder.Derived

Returns or sets the indicator if this should be marked as a derived from another datum.

-------------------------------------

Getter Method

Signature Derived()

Returns:
Return type:bool

New in version NX8.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Derived(derived)

Parameters:derived (bool) –

New in version NX8.5.0.

License requirements: ugweld (“UG WELD”)

DirectionAxis

DatumCommonBuilder.DirectionAxis

Returns or sets the direction axis.

This defines the datum origin and specifed axis.

-------------------------------------

Getter Method

Signature DirectionAxis()

Returns:
Return type:NXOpen.Axis

New in version NX8.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature DirectionAxis(directionAxis)

Parameters:directionAxis (NXOpen.Axis) –

New in version NX8.5.0.

License requirements: ugweld (“UG WELD”)

DirectionLength

DatumCommonBuilder.DirectionLength

Returns or sets the length of the datum axis vector created.

-------------------------------------

Getter Method

Signature DirectionLength()

Returns:
Return type:float

New in version NX8.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature DirectionLength(directionLength)

Parameters:directionLength (float) –

New in version NX8.5.0.

License requirements: ugweld (“UG WELD”)

ModelingTolerance

DatumCommonBuilder.ModelingTolerance

Returns or sets the modeling distance tolerance.

-------------------------------------

Getter Method

Signature ModelingTolerance()

Returns:
Return type:float

New in version NX8.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature ModelingTolerance(modelingTolerance)

Parameters:modelingTolerance (float) –

New in version NX8.5.0.

License requirements: ugweld (“UG WELD”)

PlaneHeight

DatumCommonBuilder.PlaneHeight

Returns or sets the plane height along the direction axis.

Controls the boundary of a datum plane.

-------------------------------------

Getter Method

Signature PlaneHeight()

Returns:
Return type:float

New in version NX8.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature PlaneHeight(planeHeight)

Parameters:planeHeight (float) –

New in version NX8.5.0.

License requirements: ugweld (“UG WELD”)

PlaneWidth

DatumCommonBuilder.PlaneWidth

Returns or sets the plane width perpendicular to the direction axis.

Controls the boundary of a datum plane.

-------------------------------------

Getter Method

Signature PlaneWidth()

Returns:
Return type:float

New in version NX8.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature PlaneWidth(planeWidth)

Parameters:planeWidth (float) –

New in version NX8.5.0.

License requirements: ugweld (“UG WELD”)

PrincipalAxisX

DatumCommonBuilder.PrincipalAxisX

Returns or sets the principal axis x.

Used to specify datum is controlling the x axis.

-------------------------------------

Getter Method

Signature PrincipalAxisX()

Returns:
Return type:bool

New in version NX8.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature PrincipalAxisX(principalAxisX)

Parameters:principalAxisX (bool) –

New in version NX8.5.0.

License requirements: ugweld (“UG WELD”)

PrincipalAxisY

DatumCommonBuilder.PrincipalAxisY

Returns or sets the principal axis y.

Used to specify the datum is controlling the y axis.

-------------------------------------

Getter Method

Signature PrincipalAxisY()

Returns:
Return type:bool

New in version NX8.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature PrincipalAxisY(principalAxisY)

Parameters:principalAxisY (bool) –

New in version NX8.5.0.

License requirements: ugweld (“UG WELD”)

PrincipalAxisZ

DatumCommonBuilder.PrincipalAxisZ

Returns or sets the principal axis z.

Used to specify the datum is controlling the z axis.

-------------------------------------

Getter Method

Signature PrincipalAxisZ()

Returns:
Return type:bool

New in version NX8.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature PrincipalAxisZ(principalAxisZ)

Parameters:principalAxisZ (bool) –

New in version NX8.5.0.

License requirements: ugweld (“UG WELD”)

ProjectAlongDirection

DatumCommonBuilder.ProjectAlongDirection

Returns or sets the project along direction.

Two coordiantes can be specified and the third obtained from projection.

-------------------------------------

Getter Method

Signature ProjectAlongDirection()

Returns:
Return type:bool

New in version NX8.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature ProjectAlongDirection(projectAlongDirection)

Parameters:projectAlongDirection (bool) –

New in version NX8.5.0.

License requirements: ugweld (“UG WELD”)

SectionPlaneNormal

DatumCommonBuilder.SectionPlaneNormal

Returns or sets the section plane normal.

This is sometimes referred to as the clamping plane.

-------------------------------------

Getter Method

Signature SectionPlaneNormal()

Returns:
Return type:NXOpen.Direction

New in version NX8.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature SectionPlaneNormal(sectionPlaneNormal)

Parameters:sectionPlaneNormal (NXOpen.Direction) –

New in version NX8.5.0.

License requirements: ugweld (“UG WELD”)

SolidType

DatumCommonBuilder.SolidType

Returns or sets the solid body type specified.

-------------------------------------

Getter Method

Signature SolidType()

Returns:
Return type:NXOpen.Weld.DatumCommonBuilderSolidTypes

New in version NX8.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature SolidType(solidType)

Parameters:solidType (NXOpen.Weld.DatumCommonBuilderSolidTypes) –

New in version NX8.5.0.

License requirements: ugweld (“UG WELD”)

Method Detail

UpdateWithDerivedDatum

DatumCommonBuilder.UpdateWithDerivedDatum

Initialize the builder with the inputs from an existing datum.

The builder type and derived datum type must be the same.

Signature UpdateWithDerivedDatum()

New in version NX8.5.0.

License requirements: ugweld (“UG WELD”)

Validate

DatumCommonBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.