AutoPointBuilderTypes Enumeration¶
NXOpen.Weld.AutoPointBuilder.Types is an alias for NXOpen.Weld.AutoPointBuilderTypes
-
class
NXOpen.Weld.
AutoPointBuilderTypes
¶ Bases:
object
Settings to indicate whether new features should be created, or if features will be reused.
Enum Members
Enum Member Enum Member Description New new points are being createdMove move existing points-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-