JointmarkBuilderMethod Enumeration

NXOpen.Weld.JointmarkBuilder.Method is an alias for NXOpen.Weld.JointmarkBuilderMethod

class NXOpen.Weld.JointmarkBuilderMethod

Bases: object

The type of construction method for creating Jointmark

Enum Members

Enum Member Enum Member Description
GuideCurve
Guide Curve
Mirror
Mirror
Points
Points
Translate
Translate
ExistingPoints
Existing Points. Only allowed for NXOpen.Weld.PointMark class.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.