JointmarkBuilderOrientationMethodTypes Enumeration

NXOpen.Weld.JointmarkBuilder.OrientationMethodTypes is an alias for NXOpen.Weld.JointmarkBuilderOrientationMethodTypes

class NXOpen.Weld.JointmarkBuilderOrientationMethodTypes

Bases: object

The type of orientation method for defining the default coordinate system.

Enum Members

Enum Member Enum Member Description
SurfaceNormal
Surface Normals.
CoordinateSystem
Use fixed csys instead of surface normals.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.