WeldDatumControlDirection Enumeration

class NXOpen.Weld.WeldDatumControlDirection

Bases: object

the control direction for datum Enum Members

Enum Member Enum Member Description
Invalid
Invalid direction
X
X direction
Y
Y direction
Z
Z direction
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.