WeldPointSpacingMethod Enumeration

class NXOpen.Weld.WeldPointSpacingMethod

Bases: object

Guide spacing method Enum Members

Enum Member Enum Member Description
Distance
Place multiple spot welds based on distance
NumPoints
Place multiple spot welds based on number of points
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.