WeldGrooveExtension Enumeration

class NXOpen.Weld.WeldGrooveExtension

Bases: object

Groove Extension Type Enum Members

normals from selected edges. “

ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.