WeldFeatureSetType Enumeration¶
-
class
NXOpen.Weld.
WeldFeatureSetType
¶ Bases:
object
the feature set types Enum Members
Enum Member Enum Member Description FilletWeld Fillet WeldGrooveWeld Groove WeldResistanceSpot Resistance SpotArcSpot Arc SpotClinch ClinchDollop DollopWeldNut Weld NutWeldStud Weld StudCustom1Point Custom1 PointCustom2Point Custom2 PointCustom3Point Custom3 PointCustom4Point Custom4 PointCustom5Point Custom5 PointBiwDatumSurface Datum SurfaceBiwDatumPin Datum PinBiwDatumCustomer1 Datum Customer1BiwDatumCustomer2 Datum Customer2BiwDatumCustomer3 Datum Customer3BiwMeasurementSurface Measurement SurfaceBiwMeasurementHole Measurement HoleBiwMeasurementSlot Measurement SlotBiwMeasurementStud Measurement StudBiwMeasurementTrim Measurement TrimBiwMeasurementHem Measurement HemBiwMeasurementCustomer1 Measurement Customer1BiwMeasurementCustomer2 Measurement Customer2BiwMeasurementCustomer3 Measurement Customer3-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-