WeldBeadBuilder Class¶
-
class
NXOpen.Weld.
WeldBeadBuilder
¶ Bases:
NXOpen.Builder
Used to create or edit a
NXOpen.Weld.WeldBead
feature.To create a new instance of this class, use
NXOpen.Weld.WeldManager.CreateWeldBeadBuilder()
Default values.
Property Value BeadLocation SecondaryParts TangentAngle 45.0 New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
BeadLocation | Returns or sets the desired bead location. |
Characteristics | Returns the characteristics to assign to the object created. |
DistanceTolerance | Returns or sets the distance tolerance for constructing the bead. |
ExtendToBoundary | Returns or sets the option to control if the bead guide curve should extend to the nearest face boundary. |
OutputType | Returns or sets the output type which controls the update behaviour of the bead feature. |
PathList | Returns the list containing the defined path segments. |
SelectBottomParts | Returns the collector containing the secondary bodies the bead is attached to. |
SelectTopParts | Returns the collector containing the primary bodies the bead is attached to. |
SizeList | Returns the list containing the sizes used to create the bead. |
Tag | Returns the Tag for this object. |
TangentAngle | Returns or sets the tangent angle used to find faces tangent to the seed face specified. |
Type | Returns or sets the shape of the bead to create. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GetPreviewPath | The preview curve that will be used to create the bead solid. |
NewPath | Creates a NXOpen.Weld.WeldBeadPathBuilder object. |
NewSize | Creates a NXOpen.Weld.WeldBeadSizeBuilder object. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
WeldBeadBuilderBeadLocationMethod Enumeration | Settings to indicate the desired location of the bead. |
WeldBeadBuilderOutputTypes Enumeration | Settings to indicate the update behaviour of the bead feature |
WeldBeadBuilderTypes Enumeration | Settings to indicate the sweep shape of the bead. |
Property Detail¶
BeadLocation¶
-
WeldBeadBuilder.
BeadLocation
¶ Returns or sets the desired bead location.
-------------------------------------
Getter Method
Signature
BeadLocation()
Returns: Return type: NXOpen.Weld.WeldBeadBuilderBeadLocationMethod
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BeadLocation(beadLocation)
Parameters: beadLocation ( NXOpen.Weld.WeldBeadBuilderBeadLocationMethod
) –New in version NX7.5.0.
License requirements: ugweld (“UG WELD”)
Characteristics¶
-
WeldBeadBuilder.
Characteristics
¶ Returns the characteristics to assign to the object created.
-------------------------------------
Getter Method
Signature
Characteristics()
Returns: Return type: NXOpen.Weld.CharacteristicsBuilder
New in version NX7.5.0.
License requirements: None.
DistanceTolerance¶
-
WeldBeadBuilder.
DistanceTolerance
¶ Returns or sets the distance tolerance for constructing the bead.
-------------------------------------
Getter Method
Signature
DistanceTolerance()
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DistanceTolerance(distanceTolerance)
Parameters: distanceTolerance (float) – New in version NX7.5.0.
License requirements: ugweld (“UG WELD”)
ExtendToBoundary¶
-
WeldBeadBuilder.
ExtendToBoundary
¶ Returns or sets the option to control if the bead guide curve should extend to the nearest face boundary.
-------------------------------------
Getter Method
Signature
ExtendToBoundary()
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ExtendToBoundary(extendToBoundary)
Parameters: extendToBoundary (bool) – New in version NX11.0.0.
License requirements: ugweld (“UG WELD”)
OutputType¶
-
WeldBeadBuilder.
OutputType
¶ Returns or sets the output type which controls the update behaviour of the bead feature.
-------------------------------------
Getter Method
Signature
OutputType()
Returns: Return type: NXOpen.Weld.WeldBeadBuilderOutputTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OutputType(type)
Parameters: type ( NXOpen.Weld.WeldBeadBuilderOutputTypes
) –New in version NX7.5.0.
License requirements: ugweld (“UG WELD”)
PathList¶
-
WeldBeadBuilder.
PathList
¶ Returns the list containing the defined path segments.
-------------------------------------
Getter Method
Signature
PathList()
Returns: Return type: NXOpen.Weld.WeldBeadPathBuilderList
New in version NX7.5.0.
License requirements: None.
SelectBottomParts¶
-
WeldBeadBuilder.
SelectBottomParts
¶ Returns the collector containing the secondary bodies the bead is attached to.
-------------------------------------
Getter Method
Signature
SelectBottomParts()
Returns: Return type: NXOpen.ScCollector
New in version NX7.5.0.
License requirements: None.
SelectTopParts¶
-
WeldBeadBuilder.
SelectTopParts
¶ Returns the collector containing the primary bodies the bead is attached to.
-------------------------------------
Getter Method
Signature
SelectTopParts()
Returns: Return type: NXOpen.ScCollector
New in version NX7.5.0.
License requirements: None.
SizeList¶
-
WeldBeadBuilder.
SizeList
¶ Returns the list containing the sizes used to create the bead.
-------------------------------------
Getter Method
Signature
SizeList()
Returns: Return type: NXOpen.Weld.WeldBeadSizeBuilderList
New in version NX7.5.0.
License requirements: None.
TangentAngle¶
-
WeldBeadBuilder.
TangentAngle
¶ Returns or sets the tangent angle used to find faces tangent to the seed face specified.
-------------------------------------
Getter Method
Signature
TangentAngle()
Returns: Return type: float New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TangentAngle(tangentAngle)
Parameters: tangentAngle (float) – New in version NX10.0.0.
License requirements: ugweld (“UG WELD”)
Type¶
-
WeldBeadBuilder.
Type
¶ Returns or sets the shape of the bead to create.
-------------------------------------
Getter Method
Signature
Type()
Returns: Return type: NXOpen.Weld.WeldBeadBuilderTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type(type)
Parameters: type ( NXOpen.Weld.WeldBeadBuilderTypes
) –New in version NX7.5.0.
License requirements: ugweld (“UG WELD”)
Method Detail¶
GetPreviewPath¶
-
WeldBeadBuilder.
GetPreviewPath
¶ The preview curve that will be used to create the bead solid.
Signature
GetPreviewPath()
Returns: The preview curve. Return type: NXOpen.Spline
New in version NX10.0.3.
License requirements: None.
NewPath¶
-
WeldBeadBuilder.
NewPath
¶ Creates a
NXOpen.Weld.WeldBeadPathBuilder
object.Signature
NewPath()
Returns: Return type: NXOpen.Weld.WeldBeadPathBuilder
New in version NX7.5.0.
License requirements: ugweld (“UG WELD”)
NewSize¶
-
WeldBeadBuilder.
NewSize
¶ Creates a
NXOpen.Weld.WeldBeadSizeBuilder
object.Signature
NewSize()
Returns: Return type: NXOpen.Weld.WeldBeadSizeBuilder
New in version NX7.5.0.
License requirements: ugweld (“UG WELD”)
Validate¶
-
WeldBeadBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.