WeldBeadBuilderBeadLocationMethod Enumeration

NXOpen.Weld.WeldBeadBuilder.BeadLocationMethod is an alias for NXOpen.Weld.WeldBeadBuilderBeadLocationMethod

class NXOpen.Weld.WeldBeadBuilderBeadLocationMethod

Bases: object

Settings to indicate the desired location of the bead.

Enum Members

Enum Member Enum Member Description
SecondaryParts
on the secondary parts
PrimaryParts
on the primary parts
InSpace
in space. No on any parts
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.