WeldFeatureOutput Enumeration

class NXOpen.Weld.WeldFeatureOutput

Bases: object

Feature output Enum Members

Enum Member Enum Member Description
Curves
Output only curves
Solid
Output only solids
Both
Output both curves and solids
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.