JointmarkGuideBuilderSpaceMethod Enumeration

NXOpen.Weld.JointmarkGuideBuilder.SpaceMethod is an alias for NXOpen.Weld.JointmarkGuideBuilderSpaceMethod

class NXOpen.Weld.JointmarkGuideBuilderSpaceMethod

Bases: object

Options for Spacing Method

Enum Members

Enum Member Enum Member Description
ArcLength
Arc Length
ParallelXPlane
Parallel X Plane
ParallelYPlane
Parallel Y Plane
ParallelZPlane
Parallel Z Plane
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.