PointMarkPointBuilder Class¶
-
class
NXOpen.Weld.
PointMarkPointBuilder
¶ Bases:
NXOpen.Weld.JointmarkPointsBuilder
Used to create or edit a point in the list of points for Jointmark
To create a new instance of this class, use
NXOpen.Weld.PointMarkBuilder.NewPointsOverride()
New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
Angle | Returns the angle through which X and Y axis to rotate |
FlipDirection | Returns or sets the flip of Z axis. |
MappingFeature | Returns the selected feature to move to the location specified. |
Point | Returns or sets the point at which the feature is created |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
UpdateCsys | Update the csys using a new matrix. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Method Detail¶
Validate¶
-
PointMarkPointBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.