WeldFillBuilderBoundaryMethodType Enumeration

NXOpen.Weld.WeldFillBuilder.BoundaryMethodType is an alias for NXOpen.Weld.WeldFillBuilderBoundaryMethodType

class NXOpen.Weld.WeldFillBuilderBoundaryMethodType

Bases: object

Defines whether the initial boundary of the fill pattern is defined by a two point rectangle or a curve.

Enum Members

Enum Member Enum Member Description
Rectangle
Boundary defined by a two point rectangle.
Curve
Boundary defined by a curve.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.