WeldParasetLocation Enumeration

class NXOpen.Weld.WeldParasetLocation

Bases: object

the index of user picked refsheet location Enum Members

Enum Member Enum Member Description
Length
arc length
Percent
percent arc length
ThroughPoint
through point
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.