WeldPmiBuilder Class¶
-
class
NXOpen.Weld.
WeldPmiBuilder
¶ Bases:
NXOpen.Builder
Create PMI symbols for multiple structure welds, this builder’s Commit can produce more than one object, the GetCommittedObjects can be used to get the objects and the order of GetCommittedObject’s output array is stable.
To create a new instance of this class, use
NXOpen.Weld.WeldManager.CreateWeldPmiBuilder()
Default values.
Property Value PlaneType ModelView SpaceFactor 1.0 New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
Objects | Returns the objects (either features or curves) that are used to create PMI symbols. |
PlaneType | Returns or sets the plane type. |
SpaceFactor | Returns or sets the space factor. |
Style | Returns the Annotations.StyleBuilder for the annotation. |
Tag | Returns the Tag for this object. |
UserCoordinateSystem | Returns or sets the user specified coordinate system. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
WeldPmiBuilderOrientationPlaneType Enumeration | This represents the Orientation Plane Type. |
Property Detail¶
Objects¶
-
WeldPmiBuilder.
Objects
¶ Returns the objects (either features or curves) that are used to create PMI symbols.
-------------------------------------
Getter Method
Signature
Objects()
Returns: Selected weld objects list. Return type: NXOpen.SelectNXObjectList
New in version NX9.0.0.
License requirements: None.
PlaneType¶
-
WeldPmiBuilder.
PlaneType
¶ Returns or sets the plane type.
-------------------------------------
Getter Method
Signature
PlaneType()
Returns: Return type: NXOpen.Weld.WeldPmiBuilderOrientationPlaneType
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PlaneType(planeType)
Parameters: planeType ( NXOpen.Weld.WeldPmiBuilderOrientationPlaneType
) –New in version NX9.0.0.
License requirements: ugweld (“UG WELD”) OR structure_weld (“STRUCTURE WELD”)
SpaceFactor¶
-
WeldPmiBuilder.
SpaceFactor
¶ Returns or sets the space factor.
The value is greater than zero.
-------------------------------------
Getter Method
Signature
SpaceFactor()
Returns: Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SpaceFactor(spaceFactor)
Parameters: spaceFactor (float) – New in version NX9.0.0.
License requirements: ugweld (“UG WELD”) OR structure_weld (“STRUCTURE WELD”)
Style¶
-
WeldPmiBuilder.
Style
¶ Returns the
Annotations.StyleBuilder
for the annotation.-------------------------------------
Getter Method
Signature
Style()
Returns: Return type: NXOpen.Annotations.StyleBuilder
New in version NX9.0.0.
License requirements: None.
UserCoordinateSystem¶
-
WeldPmiBuilder.
UserCoordinateSystem
¶ Returns or sets the user specified coordinate system.
-------------------------------------
Getter Method
Signature
UserCoordinateSystem()
Returns: Return type: NXOpen.CoordinateSystem
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UserCoordinateSystem(userCsys)
Parameters: userCsys ( NXOpen.CoordinateSystem
) –New in version NX9.0.0.
License requirements: ugweld (“UG WELD”) OR structure_weld (“STRUCTURE WELD”)
Method Detail¶
Validate¶
-
WeldPmiBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.