EdgePrepValuesBuilderOption Enumeration

NXOpen.Weld.EdgePrepValuesBuilder.Option is an alias for NXOpen.Weld.EdgePrepValuesBuilderOption

class NXOpen.Weld.EdgePrepValuesBuilderOption

Bases: object

Option to indicate how the values are to be used.

Enum Members

Enum Member Enum Member Description
Entered
Use the values entered as edge prep values.
Computed
Use the computed values as edge prep values.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.