WeldPointReferenceSheetType Enumeration¶
-
class
NXOpen.Weld.
WeldPointReferenceSheetType
¶ Bases:
object
Settings for the reference sheet Enum Members
Enum Member Enum Member Description Overlap spot welds are based on the intersection of face setsTop spot welds are based on the first face setNotSet spot welds are points in 3d space-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-