WeldGrooveBuilderSkipWeldMethod Enumeration

NXOpen.Weld.WeldGrooveBuilder.SkipWeldMethod is an alias for NXOpen.Weld.WeldGrooveBuilderSkipWeldMethod

class NXOpen.Weld.WeldGrooveBuilderSkipWeldMethod

Bases: object

The options for creating Skip Weld

Enum Members

Enum Member Enum Member Description
NumberLength
Number and Length
NumberSpacing
Number and Spacing
SpacingLength
Spacing and Length
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.