DatumSurfaceBuilderTypes Enumeration

NXOpen.Weld.DatumSurfaceBuilder.Types is an alias for NXOpen.Weld.DatumSurfaceBuilderTypes

class NXOpen.Weld.DatumSurfaceBuilderTypes

Bases: object

Settings to indicate the construction type used for the datum surface.

Enum Members

Enum Member Enum Member Description
Direct
direct location
Mirror
mirror location
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.