WeldTaperMethod Enumeration

class NXOpen.Weld.WeldTaperMethod

Bases: object

Settings for groove taper method Enum Members

Enum Member Enum Member Description
FromEndFace
Taper will be measured from groove end caps
FromSideFace
Taper will be measured from groove side face
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.