WeldBeadSizeBuilderTriangleMethodType Enumeration¶
NXOpen.Weld.WeldBeadSizeBuilder.TriangleMethodType is an alias for NXOpen.Weld.WeldBeadSizeBuilderTriangleMethodType
-
class
NXOpen.Weld.
WeldBeadSizeBuilderTriangleMethodType
¶ Bases:
object
Settings to indicate the type of method used to build a triangle shape.
Enum Members
Enum Member Enum Member Description LegLength Triangle defined by leg lengthsThroatThickness Trangle defined by throat thickness-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-