Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
nxopen.motion |
Provides classes and interfaces for Motion Simulation.
|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Class and Description |
---|
MarkerCollection
Represents a collection of Markers
To obtain an instance of this class, refer to Part Created in NX4.0.0 |
MotionManager
A manager to deal with all motion objects
To obtain an instance of this class, refer to Part Created in NX5.0.0 |
MotionSession |
MotionSimulation
Represents Motion.Simulation
To obtain an instance of this class, refer to Session Created in NX5.0.0 |
PackagingCollection
Represents a collection of Packaging objects
To obtain an instance of this class, refer to Part Created in NX4.0.0 |
Class and Description |
---|
ActiveView
Definitions of post articulation and spreadsheet run active view type
|
AdamsSolverProperty |
AddSubmechanismBuilder
Represents a builder class that performs add submechanism in current context.
|
AddSubmechanismBuilder.Layer
Represents initial location type that can be present during add component
|
AdoptionManager
Represents the
AdoptionManager An instance of this class can not be obtained Created in NX11.0.0 NX_REMOVE_FROM_JAVA_API |
AdoptionPair
Represents a adoption pair object
To create a new instance of this class, use AdoptionPairCollection.createPair(nxopen.NXObject, nxopen.motion.MotionObject) Created in NX11.0.0 NX_REMOVE_FROM_JAVA_API |
AdoptionPairCollection
Represents a collection of adoption pair objects
To obtain an instance of this class, refer to MotionManager Created in NX11.0.0 NX_REMOVE_FROM_JAVA_API |
AdvancedSolution
Represents a
AdvancedSolution . |
AdvancedSolutionBuilder
Represents a
AdvancedSolution builder To create a new instance of this class, use MotionSolutionCollection.createAdvancedSolutionBuilder(nxopen.motion.AdvancedSolution) Created in NX12.0.0 |
AnalyticalContact
Represents an Analytical Contact motion object.
|
AnalyticalContactBuilder
Represents a
AnalyticalContact builder To create a new instance of this class, use AnalyticalContactCollection.createAnalyticalContactBuilder(nxopen.motion.AnalyticalContact) Default values. |
AnalyticalContactBuilder.ContactTypeOption
Contact type
|
AnalyticalContactBuilder.ProfileType
Profile Type
|
AnalyticalContactCollection
Represents a collection of Analytical Contact objects
To obtain an instance of this class, refer to MotionManager Created in NX12.0.0 |
AnalyticalContactProperty
Represents an Analytical Contact Property.
|
AnalyticalContactPropertyBuilder
Represents a
AnalyticalContactProperty builder To create a new instance of this class, use AnalyticalContactPropertyCollection.createAnalyticalContactPropertyBuilder(nxopen.motion.AnalyticalContactProperty) Default values. |
AnalyticalContactPropertyBuilder.DampingType
Damping Type
|
AnalyticalContactPropertyBuilder.FrictionCoefficientType
Friction Coefficient Type
|
AnalyticalContactPropertyBuilder.StiffnessType
Stiffness Type
|
AnalyticalContactPropertyCollection
Represents a collection of Analytical Contact Property objects
To obtain an instance of this class, refer to MotionManager Created in NX12.0.0 |
AnimationControl |
ArticulationControl |
ArticulationControl.ArticulationJointsDisplacementData
This class holds the data returned from
ArticulationControl.getArticulationJointsDisplacement(nxopen.motion.Joint) |
BaseSection
Represents a base section function
To create or edit an instance of this class, use BaseSectionBuilder Created in NX12.0.0 |
BaseSectionBuilder
Represents a
BaseSectionBuilder . |
BaseSectionCollection
Represents a collection of BaseSections
To obtain an instance of this class, refer to MotionManager Created in NX12.0.0 |
BeamForce
Represents a BeamForce
To create or edit an instance of this class, use BeamForceBuilder Created in NX12.0.0 |
BeamForceBuilder
Represents a
BeamForceBuilder builder To create a new instance of this class, use BeamForceCollection.createBeamForceBuilder(nxopen.motion.BeamForce) Default values. |
BeamForceBuilder.DampingTypes
the damping type
|
BeamForceBuilder.VectorTypes
the vector direction of the beam force
|
BeamForceCollection
Represents a collection of BeamForces
To obtain an instance of this class, refer to MotionManager Created in NX12.0.0 |
BodyContact
Represents a
BodyContact
To create or edit an instance of this class, use BodyContactBuilder Created in NX5.0.0 |
BodyContactAdams |
BodyContactAdams.CoulombFriction
the enum for friction option of 3D contact
|
BodyContactAdams.ForceModel
the enum for forec model of 3D contact
|
BodyContactBuilder
Represents a
BodyContactBuilder To create a new instance of this class, use BodyContactCollection.createBodyContactBuilder(nxopen.motion.BodyContact) Default values. |
BodyContactBuilder.ContactTypeOption
the contact type (3D Contact or Sphere to CAD Contact)
|
BodyContactCollection
Represents a collection of 3D contact objects.Any contact object must
be created and found through this class
To obtain an instance of this class, refer to MotionManager Created in NX5.0.0 |
BodyContactLms |
BodyContactLms.CoulombFriction
the enum for friction option of 3D contact
|
BodyContactLms.ForceModelType
the enum for force model of 3D contact
|
BodyContactRecurdyn |
BodyContactRecurdyn.ContactType
the enum for contact type option of 3D contact
|
BodyContactRecurdyn.CoulombFriction
the enum for friction option of 3D contact
|
BodyContactRecurdyn.ForceModel
the enum for forec model of 3D contact
|
BodyContactRecurdyn.SurfaceType
the enum for surface type option of 3D contact
|
BodyContactSphereToCAD |
BodyContactSphereToCAD.CoulombFriction
the enum for friction option
|
Bushing
Represents a bushing
To create or edit an instance of this class, use BushingBuilder Created in NX6.0.0 |
BushingActuatorCoefficients
Represents a Motion BushingActuatorCoefficients
.
|
BushingBuilder
Represents a Motion BushingBuilder
To create a new instance of this class, use BushingCollection.createBushingBuilder(nxopen.motion.Bushing) Default values. |
BushingBuilder.BushingTypes
Definitions of bushing type
|
BushingCoefficients
Deprecated.
Deprecated in NX12.0.0. Use
BushingStiffnessCoefficients , BushingDampingCoefficients and BushingActuatorCoefficients instead.
|
BushingCollection
Represents a collection of motion joints
To obtain an instance of this class, refer to MotionManager Created in NX6.0.0 |
BushingCylindricalCoefficients
Represents a Motion BushingCylindricalCoefficients
.
|
BushingCylindricalCoefficientsComponent
Represents a Motion BushingCylindricalCoefficientsComponent
.
|
BushingCylindricalCoefficientTypes
Definitions of bushing cylindrical coefficient component type
|
BushingDampingCoefficients
Represents a Motion BushingDampingCoefficients
.
|
BushingDefine
Represents a Motion BushingDefine .
|
BushingDefine.AngleCalculationOption
Defines the Angle Calculation option
|
BushingDefine.ForceCalculationOption
Defines the Force Calculation option
|
BushingDefine.OrientationTypes
Defines the orientation type of bushing
|
BushingGeneralCoefficientMoveTypes
Definitions move type of general type bushing coefficient
|
BushingGeneralCoefficients
Represents a Motion BushingGeneralCoefficients
.
|
BushingGeneralCoefficientsComponent
Represents a Motion BushingGeneralCoefficientsComponent
.
|
BushingGeneralCoefficientTypes
Definitions of bushing general coefficient component type
|
BushingSphericalCoefficients
Represents a Motion BushingSphericalCoefficients
.
|
BushingSphericalCoefficientsComponent
Represents a Motion BushingSphericalCoefficientsComponent
.
|
BushingSphericalCoefficientTypes
Definitions of bushing spherical coefficient component type
|
BushingStiffnessCoefficients
Represents a Motion BushingStiffnessCoefficients
.
|
ConfigurationParameter
Represents a
ConfigurationParameter . |
ConfigurationParameterList
Represents a list of objects.
|
Connector
Represents a connector
This is an abstract class, and cannot be created. |
ConnectorBuilder
Represents ConnectorBuilder
This is an abstract class, and cannot be created. |
ConnectorBuilder.ApplicationDirection
Definitions of application direction
|
ConnectorBuilder.AttachmentType
Definitions of connector attachment type
|
ConnectorCoefficientTypes
Definitions of connector coefficient type
|
ControlInput
Represents a Control Input motion object.
|
ControlInputBuilder
Represents a
ControlInput builder To create a new instance of this class, use ControlInputCollection.createControlInputBuilder(nxopen.motion.ControlInput) Created in NX11.0.0 |
ControlInputBuilder.InputType
Control Input type
|
ControlInputCollection
Represents a collection of Control Input objects
To obtain an instance of this class, refer to MotionManager Created in NX11.0.0 |
ControlInputPortBuilder
Represents a
ControlPort builder specific to control input element. |
ControlInputPortBuilder.MeasuredComponent
the types of components that can be measured by the control input element for the selected variable.
|
ControlInputPortBuilder.MeasuredVariable
the types of variables that can be measured by the control input element.
|
ControlInputPortBuilderList
Represents a list of objects.
|
ControlOutput
Represents a Control Output motion object.
|
ControlOutputBuilder
Represents a
ControlOutput builder To create a new instance of this class, use ControlOutputCollection.createControlOutputBuilder(nxopen.motion.ControlOutput) Default values. |
ControlOutputBuilder.ControlOutputType
Control Output type
|
ControlOutputBuilder.DirectionType
Output Variable Direction
|
ControlOutputBuilder.VariableType
Output Variable type
|
ControlOutputCollection
Represents a collection of Control Output objects
To obtain an instance of this class, refer to MotionManager Created in NX11.0.0 |
ControlPort
Represents a motion control port object class.
|
ControlPortCollection
Represents a collection of Control Port objects
To obtain an instance of this class, refer to ControlInput Created in NX11.0.0 |
Coupler
Represents a motion coupler object
This is an abstract class, and cannot be created. |
CouplerBuilder
Represents a
CouplerBuilder This is an abstract class, and cannot be created. |
CouplerCable
Represents a motion cable object
To create or edit an instance of this class, use CouplerCableBuilder Created in NX6.0.0 |
CouplerCableBuilder
Represents a
CouplerCableBuilder To create a new instance of this class, use CouplerCollection.createCouplerCableBuilder(nxopen.motion.CouplerCable) Created in NX6.0.0 |
CouplerCollection
Represents a collection of motion couplers
To obtain an instance of this class, refer to MotionManager Created in NX6.0.0 |
CouplerGear
Represents a motion gear object
To create or edit an instance of this class, use CouplerGearBuilder Created in NX6.0.0 |
CouplerGearBuilder
Represents a
CouplerGearBuilder To create a new instance of this class, use CouplerCollection.createCouplerGearBuilder(nxopen.motion.CouplerGear) Created in NX6.0.0 |
CouplerRckpn
Represents a motion rack and pinion object
To create or edit an instance of this class, use CouplerRckpnBuilder Created in NX6.0.0 |
CouplerRckpnBuilder
Represents a
CouplerRckpnBuilder To create a new instance of this class, use CouplerCollection.createCouplerRckpnBuilder(nxopen.motion.CouplerRckpn) Created in NX6.0.0 |
CurveContact
Represents a
CurveContact
To create or edit an instance of this class, use CurveContactBuilder Created in NX5.0.0 |
CurveContactAdams |
CurveContactBuilder
Represents a
CurveContactBuilder To create a new instance of this class, use CurveContactCollection.createCurveContactBuilder(nxopen.motion.CurveContact) Default values. |
CurveContactBuilder.GeometryMaterialSide
the enum for the materia side direction of the selected geometry
|
CurveContactCollection
Represents a collection of 2D contact objects.Any 2D contact object must
be created and found through this class
To obtain an instance of this class, refer to MotionManager Created in NX5.0.0 |
CurveContactRecurdyn |
CurveOnCurve
Represents a curve on curve
To create or edit an instance of this class, use CurveOnCurveBuilder Created in NX6.0.0 |
CurveOnCurveBuilder
Represents a
CurveOnCurveBuilder
To create a new instance of this class, use CurveOnCurveCollection.createCurveOnCurveBuilder(nxopen.motion.CurveOnCurve) Created in NX6.0.0 |
CurveOnCurveCollection
Represents a collection of curve on curve objects
To obtain an instance of this class, refer to MotionManager Created in NX6.0.0 |
CurveParameterizedTypes
Defines curve parameterized type
|
CustomizedMaterialBuilder
Represents a
CustomizedMaterialBuilder . |
Damper
Represents a damper
To create or edit an instance of this class, use DamperBuilder Created in NX6.0.0 |
DamperBuilder
Represents a DamperBuilder
To create a new instance of this class, use DamperCollection.createDamperBuilder(nxopen.motion.Damper) Created in NX6.0.0 |
DamperCollection
Represents a collection of motion damper
To obtain an instance of this class, refer to MotionManager Created in NX6.0.0 |
DriverMotionsData |
DriverMotionsData.DriverDataType
Driver Data Type
|
DriverMotionsData.DriverRotationType
Driver Rotation type
|
DriverMultiOperations |
DriverOperation |
DriverOperation.IntegrationType
Integration type
|
DriverOperation.Type
Driver operation type
|
ExpressionFunctionBuilder
Represents a ExpressionFunctionBuilder builder .
|
ExpressionFunctionBuilder.Type
The block type can be Expression when a constant expression is used or Function when a spline curve is used or
Profile when a profile is used.
|
FieldData
Represents a FieldData
To create a new instance of this class, use FieldDataCollection.createFieldData(nxopen.fields.Field) Created in NX11.0.1 NX_REMOVE_FROM_JAVA_API |
FieldDataCollection
Represents a collection of motion joints
To obtain an instance of this class, refer to MotionManager Created in NX11.0.1 NX_REMOVE_FROM_JAVA_API |
FlexBody
Represents the Motion FlexBody class.It must be associated
with a Motion Link.
|
FlexBodyBuilder
Represents a
FlexBody builder To create a new instance of this class, use FlexBodyCollection.createFlexBodyBuilder(nxopen.motion.FlexBody) Default values. |
FlexBodyBuilder.Positioning
Represents positioning type of flexible body
|
FlexBodyBuilder.SourceType
Represents rfi file type of flexible body
|
FlexBodyBuilder.UnitSystemType
Represents unit system
|
FlexBodyCollection
Represents a collection of flexible body objects
To obtain an instance of this class, refer to MotionManager Created in NX7.5.0 |
FlexPhysicalDampingSettings
Represents the physical damping settings for flexible body .
|
ForceValueTypes
Defines function value type
|
GcouplerMovementTypes
Defines 2-3 joint coupler joint movement type
|
GeneralCoupler
Represents motion 2-3 joint coupler
To create or edit an instance of this class, use GeneralCouplerBuilder Created in NX7.5.0 |
GeneralCouplerBuilder
Represents a
GeneralCouplerBuilder To create a new instance of this class, use GeneralCouplerCollection.createGeneralCouplerBuilder(nxopen.motion.GeneralCoupler) Default values. |
GeneralCouplerBuilder.AttachmentType
Definitions of joint coupler attachment type
|
GeneralCouplerCollection
Represents a collection of 2-3 joint coupler objects
To obtain an instance of this class, refer to MotionManager Created in NX7.5.0 |
Graph
Represents a graph, only creation is supported
To create or edit an instance of this class, use GraphObjectBuilder Created in NX5.0.0 |
GraphBuilder
Deprecated.
Deprecated in NX11.0.0. Use
GraphObjectBuilder instead.
|
GraphBuilder.ComponentChoices
Deprecated.
Component attribute of the curve data.
|
GraphBuilder.CsysChoices
Deprecated.
Csys attribute of the curve data.
|
GraphBuilder.CurveData
Deprecated.
Contains the structure of curve associated with curve data.
|
GraphBuilder.PlotStyleChoices
Deprecated.
Plot output type
|
GraphBuilder.RequestChoices
Deprecated.
Request attribute of the curve data.
|
GraphBuilder.XAxisTypeChoices
Deprecated.
X axis type choice.
|
GraphManager
Represents a collection of Graph objects, only creation is supported
To obtain an instance of this class, refer to MotionManager Created in NX5.0.0 |
GraphObjectBuilder
Represents a
GraphObjectBuilder ,
only creation is supported
To create a new instance of this class, use GraphManager.createGraphObjectBuilder(nxopen.motion.Graph) Created in NX11.0.0 |
GraphObjectBuilder.QuantityTypesData
This class holds the data returned from
GraphObjectBuilder.getQuantityTypes() |
IGraphSource
Represents an interface IGraphSource .
|
InputPortAssociation
Represents a
InputPortAssociation . |
InputPortAssociationList
Represents a list of objects.
|
IPostControl
Represents an interface IPostControl .
|
Joint
Represents a motion joint object
To create or edit an instance of this class, use JointBuilder Created in NX5.0.0 |
JointBuilder
This builder class is used to create or edit
Joint objects. |
JointCollection
Represents a collection of motion joints
To obtain an instance of this class, refer to MotionManager Created in NX5.0.0 |
JointDefine
Represents a joint define object .
|
JointDefine.OrientationType
Defines the orientation type of joint
|
JointDefine.ScrewJointDisplCurveType
Defines the displacement curve type for screw joints
|
JointDefine.ScrewJointMethodType
Defines the method type of screw joints
|
JointDefine.ScrewJointRatioType
Defines the ratio type for screw joints
|
JointDefine.Type
Joint define type
|
JointDefine.UniversalJointAxisType
Defines the axis type for universal joints
|
JointDriver
Represents a joint driver
To create or edit an instance of this class, use JointDriverBuilder Created in NX5.0.0 |
JointDriverBuilder
Represents a
JointDriverBuilder
To create a new instance of this class, use JointDriverCollection.createJointDriverBuilder(nxopen.motion.JointDriver) Created in NX5.0.0 |
JointDriverCollection
Represents a collection of Driver objects
To obtain an instance of this class, refer to MotionManager Created in NX5.0.0 |
JointFriction
Represents a joint friction object .
|
JointFrictionAdams
Represents a adams joint friction object .
|
JointFrictionAdams.FrictionEffect
Joint friction effect
|
JointFrictionAdams.FrictionOverlapDelta
Joint friction overlap_delta
|
JointFrictionAdams.FrictionYokeType
Joint friction yoke type
|
JointFrictionLms
Represents a lms joint friction object .
|
JointFrictionRecurDyn
Represents a recurdyn joint friction object .
|
JointFrictionRecurDyn.FrictionEffect
Joint friction effect
|
JointFrictionRecurDyn.FrictionOverlapDelta
Joint friction overlap_delta
|
JointFrictionRecurDyn.FrictionYokeType
Joint friction yoke type
|
Link
Represents the Motion Link class.
|
LinkAttachmentData
Represents a
LinkAttachmentData . |
LinkBuilder
Represents a
LinkBuilder
To create a new instance of this class, use LinkCollection.createLinkBuilder(nxopen.motion.Link) Created in NX5.0.0 |
LinkCollection
Represents a collection of motion joints
To obtain an instance of this class, refer to MotionManager Created in NX5.0.0 |
LinkCoupler
Represents a
LinkCoupler To create or edit an instance of this class, use LinkCouplerBuilder Created in NX12.0.0 |
LinkCouplerBuilder
Represents a
LinkCouplerBuilder To create a new instance of this class, use LinkCouplerCollection.createLinkCouplerBuilder(nxopen.motion.LinkCoupler) Default values. |
LinkCouplerBuilder.CurveChoices
the LinkCoupler Curve type.
|
LinkCouplerBuilder.MethodChoices
the LinkCoupler method.
|
LinkCouplerBuilder.TypeChoices
the LinkCoupler type.
|
LinkCouplerCollection
Represents a collection of LinkCoupler objects
To obtain an instance of this class, refer to MotionManager Created in NX12.0.0 |
LinkCouplerCoupleBuilder |
LinkCouplerCoupleBuilder.MeasurementChoices
the Measurement type.
|
LinkCouplerCoupleBuilder.ScaleChoices
the Scale type.
|
LinkDriver
Represents a Link Driver
To create or edit an instance of this class, use LinkDriverBuilder Created in NX11.0.0 |
LinkDriverBuilder
Represents a
LinkDriverBuilder
To create a new instance of this class, use LinkDriverCollection.createLinkDriverBuilder(nxopen.motion.LinkDriver) Created in NX11.0.0 |
LinkDriverCollection
Represents a collection of LinkDriver objects
To obtain an instance of this class, refer to MotionManager Created in NX11.0.0 |
LinkInitialVelocity |
LinkInitialVelocity.AngularVelocityType
Defines rotate type of initial velocity.
|
LinkMassProperty |
LinkMassProperty.MassPropertyType
Defines mass property type of link
|
LmsSolverProperty |
LmsSolverProperty.DynamicAccelerationMethods
dynamic acceleration method
|
LmsSolverProperty.DynamicInitialVelocityMethods
dynamic initial velocity method
|
LmsSolverProperty.RoadHeightAdjustmentTypes
road height adjustment type
|
LmsSolverProperty.StaticJacobianTypes
static jacobian type
|
LoadTransfer
Represents a Motion Load Transfer class
To create or edit an instance of this class, use LoadTransferBuilder Created in NX9.0.0 |
LoadTransferBuilder
Represents a
LoadTransferBuilder To create a new instance of this class, use LoadTransferCollection.createLoadTransferBuilder(nxopen.motion.LoadTransfer) Default values. |
LoadTransferCollection
Represents a collection of load transfer objects
To obtain an instance of this class, refer to MotionManager Created in NX9.0.0 |
LoadTransferControl |
Marker
Represents the Motion Marker class.
|
Marker.MarkerType
Marker subtype
|
MarkerBuilder
Represents a builder of Marker
To create a new instance of this class, use MarkerCollection.createMarkerBuilder(nxopen.motion.Marker) Default values. |
MarkerToNodeData |
MechanismExport
Represents a Mechanism Export object used to export one or more Motion objects to a text file.
|
MechanismExport.PositionOrientationFormat
Format to export the position and orientation data.
|
MechanismImport
Represents a Mechanism Import object used to import a Motion model from a text file.
|
MechanismImport.NamingRule
Naming Rule type to modify imported object's name
|
Mechatronics
Represents a
Mechatronics . |
MechatronicsBuilder
Represents a
Mechatronics builder To create a new instance of this class, use MechatronicsCollection.createMechatronicsBuilder(nxopen.motion.Mechatronics) Default values. |
MechatronicsBuilder.MechatronicsModelType
the mechatronics type - possible values are Matlab or Amesim
|
MechatronicsBuilder.PurposeType
the mechatronics purpose type - possible values are Import and Export
|
MechatronicsBuilder.SolverCommunicationIntervalType
the mechatronics communication interval type - only for Amesim!
|
MechatronicsBuilder.SolverIntegrationType
the mechatronics integration type - possible values are ModelExchange and CoSimulation
|
MechatronicsCollection
Represents a collection of Mechatronics
To obtain an instance of this class, refer to MotionManager Created in NX11.0.0 |
MechatronicsPortCollection
Represents a collection of ports used as outputs by Mechatronics
To obtain an instance of this class, refer to Mechatronics Created in NX11.0.0 |
MotionBuilder
This builder class is used to create or edit
MotionObject This is an abstract class, and cannot be created. |
MotionEnvironment
Represents a Motion Environment
To obtain an instance of this class, refer to MotionSession Created in NX7.5.0 |
MotionEnvironment.AdoptAssemblyJointStatus
Represents the on-off status of adopt assembly joint
|
MotionEnvironment.Analysis
Represents analysis type of current mechanisms
|
MotionEnvironment.JointWizardStatus
Represents the on-off status of joint wizard
|
MotionEnvironment.Solver
Represents Motion solver of current mechanism
|
MotionFunction
Represents a Motion Function Object
To create or edit an instance of this class, use FunctionBuilder Created in NX11.0.0 |
MotionMethods
Represents a
MotionMethods class To obtain an instance of this class, refer to MotionSession Created in NX8.0.0 |
MotionObject
Represents the motion base object class.
|
MotionObject.GroupType
The group type attribute is used for import subassembly functionality.
|
MotionSensor
Represents a motion sensor
To create or edit an instance of this class, use MotionSensorBuilder Created in NX6.0.0 |
MotionSensorBuilder
Represents a
MotionSensorBuilder
To create a new instance of this class, use MotionSensorCollection.createMotionSensorBuilder(nxopen.motion.MotionSensor) Default values. |
MotionSensorBuilder.Component
component enumeration type
|
MotionSensorBuilder.Reference
reference frame enumeration type
|
MotionSensorBuilder.Types
sensor type
|
MotionSensorCollection
Represents a collection of sensor objects
To obtain an instance of this class, refer to MotionManager Created in NX6.0.0 |
MotionSolution
Represents a solution
To create or edit an instance of this class, use MotionSolutionBuilder Created in NX5.0.0 |
MotionSolution.GraphObjectResultData
This class holds the data returned from
MotionSolution.getGraphObjectResult(nxopen.motion.Graph) |
MotionSolutionBuilder
Represents a
MotionSolutionBuilder
To create a new instance of this class, use MotionSolutionCollection.createSolutionBuilder(nxopen.motion.MotionSolution) Created in NX5.0.0 |
MotionSolutionBuilder.AnalysisTypes
Analysis type
The LMS Solver does not support
MotionSolutionBuilder.AnalysisTypes.CONTROL . |
MotionSolutionBuilder.SolutionTypes
Solution type
|
MotionSolutionCollection
Represents a collection of Driver objects
To obtain an instance of this class, refer to MotionManager Created in NX5.0.0 |
Motor
Represents a motion motor base object class
This is an abstract class, and cannot be created. |
MotorBuilder
This builder class is used to create or edit
Motor This is an abstract class, and cannot be created. |
NormalModeProperty
Represents the properties of one normal mode .
|
OutputPortAssociation
Represents a
OutputPortAssociation . |
OutputPortAssociationList
Represents a list of objects.
|
Packaging
This class is an abstract class and base class for
PackagingMeasure ,
PackagingTrace and PackagingInterference objects. |
PackagingBuilder
This class an abstract class and base class for
PackagingMeasureBuilder ,
PackagingTraceBuilder and PackagingInterferenceBuilder . |
PackagingInterference
This class represents a Packaging Interference object.
|
PackagingInterferenceBuilder
This the builder class to create or edit an Interference object.
|
PackagingInterferenceBuilder.Action
Interference action type
|
PackagingInterferenceBuilder.Frame
Interference solid reference frame type.
|
PackagingInterferenceBuilder.Mode
Interference calculation mode type
|
PackagingMeasure
This class represents a Packaging Measure object.
|
PackagingMeasureBuilder
This is the builder class to create or edit a Measure object.
|
PackagingMeasureBuilder.GeometryData
Represents geometry data.
|
PackagingMeasureBuilder.MeasureCondition
Measure condition
|
PackagingMeasureBuilder.MeasureType
Measure type
|
PackagingTrace
This class represents a Packaging Trace object.
|
PackagingTraceBuilder
This is the builder class to create or edit a Trace object.
|
PackagingTraceBuilder.Frame
Trace reference frame type
|
ParamRedefineState
Defines the redefine state of a property of an occurrence of an object in the assembly.
|
PhysicsConversionBuilder
Represents a
PhysicsConversionBuilder builder To create a new instance of this class, use MotionSession.createPhysicsConversionBuilder(nxopen.NXObject) Created in NX8.0.0 |
PhysicsConversionBuilder.PhysicsData
This class holds the data returned from
PhysicsConversionBuilder.getPhysics() |
PlantInput
Represents a Plant Input motion object
To create or edit an instance of this class, use PlantInputBuilder Created in NX6.0.0 |
PlantInputBuilder
Represents a
PlantInput builder To create a new instance of this class, use PlantInputCollection.createPlantInputBuilder(nxopen.motion.PlantInput) Created in NX6.0.0 |
PlantInputCollection
Represents a collection of Plant Input objects
To obtain an instance of this class, refer to MotionManager Created in NX6.0.0 |
PlantOutput
Represents a Plant Output motion object
To create or edit an instance of this class, use PlantOutputBuilder Created in NX6.0.0 |
PlantOutputBuilder
Represents a
PlantOutput builder To create a new instance of this class, use PlantOutputCollection.createPlantOutputBuilder(nxopen.motion.PlantOutput) Created in NX6.0.0 |
PlantOutputBuilder.Poutype
the type enum
|
PlantOutputCollection
Represents a collection of Plant Output objects
To obtain an instance of this class, refer to MotionManager Created in NX6.0.0 |
PlayMode
Definitions of post animation and spreadsheet run play mode type
|
PMDCMotor
Represents a motion pmdc motor object
To create or edit an instance of this class, use PMDCMotorBuilder Created in NX6.0.0 |
PMDCMotorBuilder
Represents a
PMDCMotorBuilder To create a new instance of this class, use PMDCMotorCollection.createPmdcMotorBuilder(nxopen.motion.PMDCMotor) Created in NX6.0.0 |
PMDCMotorBuilder.Type
Motor type
|
PMDCMotorCollection
Represents a collection of motion pmdc motor
To obtain an instance of this class, refer to MotionManager Created in NX6.0.0 |
PointOnCurve
Represents a point on curve
To create or edit an instance of this class, use PointOnCurveBuilder Created in NX6.0.0 |
PointOnCurveBuilder
Represents a
PointOnCurveBuilder
To create a new instance of this class, use PointOnCurveCollection.createPointOnCurveBuilder(nxopen.motion.PointOnCurve) Default values. |
PointOnCurveCollection
Represents a collection of point on curve objects
To obtain an instance of this class, refer to MotionManager Created in NX6.0.0 |
PointOnSurface
Represents a point on surface motion object
To create or edit an instance of this class, use PointOnSurfaceBuilder Created in NX6.0.0 |
PointOnSurfaceBuilder
Represents a
PointOnSurfaceBuilder
To create a new instance of this class, use PointOnSurfaceCollection.createPointOnSurfaceBuilder(nxopen.motion.PointOnSurface) Created in NX6.0.0 |
PointOnSurfaceCollection
Represents a collection of Point on Surface objects
To obtain an instance of this class, refer to MotionManager Created in NX6.0.0 |
PortAssociation
Represents a
PortAssociation . |
PortVariable
Represents a
PortVariable . |
PortVariableCollection
Represents a collection of ports used to expose results on Mechatronics port variables
To obtain an instance of this class, refer to Mechatronics Created in NX11.0.0 |
PortVariableList
Represents a list of objects.
|
PostControl
Represent abstract class Motion.PostControl
This is an abstract class, and cannot be instantiated. |
PostProcess
Represents the motion post process
To obtain an instance of this class, refer to MotionSession Created in NX7.5.0 |
PostProcess.CreateEnvelopeData |
PostProcess.EnvelopeAccuracyModes
The modes for envelope accuracy
|
PostProcess.EnvelopeTolerance
Contains settings for envelope tolerance
|
PostProcess.EnvelopeToleranceTypes
Envelope tolerance types
|
PostProcess.UserFunctionBeforeDialogDestroy
Post process user function callback before dialog destroy, This callback function will be call when user click the user button.
|
PostToolsControl
Represent abstract class Motion.PostToolsControl
An instance of this class can not be obtained Created in NX11.0.0 |
RecurdynSolverProperty |
RecurdynSolverProperty.StaticIntegratorTypes
Integrator type
|
ResultMeasure
Represents a result measure motion object
To create or edit an instance of this class, use ResultMeasureBuilder Created in NX11.0.0 |
ResultMeasure.InterferenceType
Result measure interference result type
|
ResultMeasure.ResultType
Result measure result type
|
ResultMeasureBuilder
Represents a
ResultMeasure builder To create a new instance of this class, use ResultMeasureCollection.createResultMeasureBuilder(nxopen.motion.ResultMeasure) Created in NX11.0.0 |
ResultMeasureCollection
Represents a collection of result measure objects
To obtain an instance of this class, refer to MotionManager Created in NX11.0.0 |
Road |
RoadBuilder
Represents a
RoadBuilder
To create a new instance of this class, use RoadCollection.createRoadBuilder(nxopen.motion.Road) Created in NX11.0.0 |
RoadBuilder.PathDatatypeChoices
data type attribute of the path data
|
RoadBuilder.SplineDatatypeChoices
data type attribute of the spline data
|
RoadBuilder.SurfaceDatatypeChoices
data type attribute of the surface data
|
RoadBuilder.TypeChoices
type attribute of the road
|
RoadCollection
Represents a collection of Road objects
To obtain an instance of this class, refer to MotionManager Created in NX11.0.0 |
ScalarForce
Represents the Motion ScalarForce class.
|
ScalarForceBuilder
Represents a
ScalarForceBuilder To create a new instance of this class, use ScalarForceCollection.createScalarForceBuilder(nxopen.motion.ScalarForce) Created in NX6.0.0 |
ScalarForceBuilder.ApplicationType
the application type.
|
ScalarForceBuilder.DirectionType
the Direction type.
|
ScalarForceCollection
Represents a Scalar Force Collection.
|
ScalarTorque
Represents the Motion ScalarTorque class.
|
ScalarTorqueBuilder
Represents a
ScalarTorqueBuilder To create a new instance of this class, use ScalarTorqueCollection.createScalarTorqueBuilder(nxopen.motion.ScalarTorque) Created in NX6.0.0 |
ScalarTorqueBuilder.AppType
the application type
|
ScalarTorqueBuilder.DirectionType
the direction
|
ScalarTorqueBuilder.ScalarTorqueType
the torque type
|
ScalarTorqueCollection
Represents a collection of motion scalar torque
To obtain an instance of this class, refer to MotionManager Created in NX6.0.0 |
Segment
Represents a segment, only creation is supported
This is created by road. |
SegmentBuilder
Represents a
SegmentBuilder ,
only creation is supported
To create a new instance of this class, use RoadBuilder.createSegmentBuilder() Created in NX11.0.0 |
SegmentBuilder.SplineDatatypeChoices
data type attribute of the straight data
|
SegmentBuilder.StraightTransitionTypeChoices
data type attribute of the straight data
|
SegmentBuilder.TypeChoices
type attribute of the segment
|
SegmentBuilderList
Represents a list of objects.
|
SegmentCollection
Represents a collection of Segment objects, only creation is supported
To obtain an instance of this class, refer to Road Created in NX11.0.0 |
SelectAnalyticalContactProperty
Represents a single object selection.
|
SelectAnalyticalContactProperty.ValueData
This class holds the data returned from
SelectAnalyticalContactProperty.getValue() |
SelectAnalyticalContactProperty.ValueWithCaeSetObjectInfoData
This class holds the data returned from
SelectAnalyticalContactProperty.getValue() |
SelectAnalyticalContactProperty.ValueWithSnapData
This class holds the data returned from
SelectAnalyticalContactProperty.getValue() |
SelectBaseSection
Represents a single object selection.
|
SelectBaseSection.ValueData
This class holds the data returned from
SelectBaseSection.getValue() |
SelectBaseSection.ValueWithCaeSetObjectInfoData
This class holds the data returned from
SelectBaseSection.getValue() |
SelectBaseSection.ValueWithSnapData
This class holds the data returned from
SelectBaseSection.getValue() |
SelectControlPort
Represents a single object selection.
|
SelectControlPort.ValueData
This class holds the data returned from
SelectControlPort.getValue() |
SelectControlPort.ValueWithCaeSetObjectInfoData
This class holds the data returned from
SelectControlPort.getValue() |
SelectControlPort.ValueWithSnapData
This class holds the data returned from
SelectControlPort.getValue() |
SelectFieldData
Represents a single object selection.
|
SelectFieldData.ValueData
This class holds the data returned from
SelectFieldData.getValue() |
SelectFieldData.ValueWithCaeSetObjectInfoData
This class holds the data returned from
SelectFieldData.getValue() |
SelectFieldData.ValueWithSnapData
This class holds the data returned from
SelectFieldData.getValue() |
SelectJoint
Represents a single object selection.
|
SelectJoint.ValueData
This class holds the data returned from
SelectJoint.getValue() |
SelectJoint.ValueWithCaeSetObjectInfoData
This class holds the data returned from
SelectJoint.getValue() |
SelectJoint.ValueWithSnapData
This class holds the data returned from
SelectJoint.getValue() |
SelectLink
Represents a single object selection.
|
SelectLink.ValueData
This class holds the data returned from
SelectLink.getValue() |
SelectLink.ValueWithCaeSetObjectInfoData
This class holds the data returned from
SelectLink.getValue() |
SelectLink.ValueWithSnapData
This class holds the data returned from
SelectLink.getValue() |
SelectMarker
Represents a single object selection.
|
SelectMarker.ValueData
This class holds the data returned from
SelectMarker.getValue() |
SelectMarker.ValueWithCaeSetObjectInfoData
This class holds the data returned from
SelectMarker.getValue() |
SelectMarker.ValueWithSnapData
This class holds the data returned from
SelectMarker.getValue() |
SelectRoad
Represents a single object selection.
|
SelectRoad.ValueData
This class holds the data returned from
SelectRoad.getValue() |
SelectRoad.ValueWithCaeSetObjectInfoData
This class holds the data returned from
SelectRoad.getValue() |
SelectRoad.ValueWithSnapData
This class holds the data returned from
SelectRoad.getValue() |
SelectSplineBeamProperty
Represents a single object selection.
|
SelectSplineBeamProperty.ValueData
This class holds the data returned from
SelectSplineBeamProperty.getValue() |
SelectSplineBeamProperty.ValueWithCaeSetObjectInfoData
This class holds the data returned from
SelectSplineBeamProperty.getValue() |
SelectSplineBeamProperty.ValueWithSnapData
This class holds the data returned from
SelectSplineBeamProperty.getValue() |
SelectTirePropertyBasic
Represents a single object selection.
|
SelectTirePropertyBasic.ValueData
This class holds the data returned from
SelectTirePropertyBasic.getValue() |
SelectTirePropertyBasic.ValueWithCaeSetObjectInfoData
This class holds the data returned from
SelectTirePropertyBasic.getValue() |
SelectTirePropertyBasic.ValueWithSnapData
This class holds the data returned from
SelectTirePropertyBasic.getValue() |
SelectTirePropertyCd
Represents a single object selection.
|
SelectTirePropertyCd.ValueData
This class holds the data returned from
SelectTirePropertyCd.getValue() |
SelectTirePropertyCd.ValueWithCaeSetObjectInfoData
This class holds the data returned from
SelectTirePropertyCd.getValue() |
SelectTirePropertyCd.ValueWithSnapData
This class holds the data returned from
SelectTirePropertyCd.getValue() |
SelectTirePropertyFt
Represents a single object selection.
|
SelectTirePropertyFt.ValueData
This class holds the data returned from
SelectTirePropertyFt.getValue() |
SelectTirePropertyFt.ValueWithCaeSetObjectInfoData
This class holds the data returned from
SelectTirePropertyFt.getValue() |
SelectTirePropertyFt.ValueWithSnapData
This class holds the data returned from
SelectTirePropertyFt.getValue() |
SelectTirePropertyMotorcycle
Represents a single object selection.
|
SelectTirePropertyMotorcycle.ValueData
This class holds the data returned from
SelectTirePropertyMotorcycle.getValue() |
SelectTirePropertyMotorcycle.ValueWithCaeSetObjectInfoData
This class holds the data returned from
SelectTirePropertyMotorcycle.getValue() |
SelectTirePropertyMotorcycle.ValueWithSnapData
This class holds the data returned from
SelectTirePropertyMotorcycle.getValue() |
SelectTirePropertyNonInertial
Represents a single object selection.
|
SelectTirePropertyNonInertial.ValueData
This class holds the data returned from
SelectTirePropertyNonInertial.getValue() |
SelectTirePropertyNonInertial.ValueWithCaeSetObjectInfoData
This class holds the data returned from
SelectTirePropertyNonInertial.getValue() |
SelectTirePropertyNonInertial.ValueWithSnapData
This class holds the data returned from
SelectTirePropertyNonInertial.getValue() |
SelectTirePropertyTno
Represents a single object selection.
|
SelectTirePropertyTno.ValueData
This class holds the data returned from
SelectTirePropertyTno.getValue() |
SelectTirePropertyTno.ValueWithCaeSetObjectInfoData
This class holds the data returned from
SelectTirePropertyTno.getValue() |
SelectTirePropertyTno.ValueWithSnapData
This class holds the data returned from
SelectTirePropertyTno.getValue() |
SignalChart
Represents a motion Signal Chart object
To create or edit an instance of this class, use SignalChartBuilder Created in NX6.0.0 |
SignalChartBuilder
Represents a
SignalChartBuilder To create a new instance of this class, use SignalChartCollection.createSignalChartBuilder(nxopen.motion.SignalChart) Created in NX6.0.0 |
SignalChartBuilder.Type
SignalChart type
|
SignalChartCollection
Represents a collection of motion Signal Chart
To obtain an instance of this class, refer to MotionManager Created in NX6.0.0 |
SignalChartListItem
Represents a SignalChartListItem,
List Item inside a SignalChartBuilder
To create a new instance of this class, use SignalChartCollection.createSignalChartListItem() Created in NX6.0.0 |
SignalChartListItem.Condition
signal chart list item condition
|
SignalChartListItem.Timer
time sensor
|
SignalChartListItemList
Represents a list of objects.
|
SplineBeam
Represents a SplineBeam
To create or edit an instance of this class, use SplineBeamBuilder Created in NX12.0.0 |
SplineBeamBuilder
Represents a
SplineBeamBuilder builder To create a new instance of this class, use SplineBeamCollection.createSplineBeamBuilder(nxopen.motion.SplineBeam) Default values. |
SplineBeamBuilder.DefinitionMethodType
the definition method type
|
SplineBeamBuilder.SectionAxisType
the definition of the section axis type
|
SplineBeamCollection
Represents a collection of SplineBeams
To obtain an instance of this class, refer to MotionManager Created in NX12.0.0 |
SplineBeamProperty
Represents a SplineBeam Property
To create or edit an instance of this class, use SplineBeamPropertyBuilder Created in NX12.0.0 |
SplineBeamPropertyBuilder
Represents a
SplineBeamPropertyBuilder builder To create a new instance of this class, use SplineBeamPropertyCollection.createSplineBeamPropertyBuilder(nxopen.motion.SplineBeamProperty) Default values. |
SplineBeamPropertyBuilder.DampingTypes
the damping type
|
SplineBeamPropertyCollection
Represents a collection of SplineBeamProperty
To obtain an instance of this class, refer to MotionManager Created in NX12.0.0 |
SpreadsheetRunControl
Represents the
SpreadsheetRunControl An instance of this class can not be obtained Created in NX9.0.0 |
Spring
Represents a spring
To create or edit an instance of this class, use SpringBuilder Created in NX6.0.0 |
SpringBuilder
Represents a SpringBuilder
To create a new instance of this class, use SpringCollection.createSpringBuilder(nxopen.motion.Spring) Default values. |
SpringCollection
Represents a collection of motion spring
To obtain an instance of this class, refer to MotionManager Created in NX6.0.0 |
StandardSection
Represents a standard beam section
To create or edit an instance of this class, use StandardSectionBuilder Created in NX12.0.0 |
StandardSectionBuilder
Represents a
StandardSectionBuilder . |
StandardSectionBuilder.StandardSectionType
the standard section type
|
SubmechanismPositioner
Represents a Submechanism Positioner object.
|
SubmechanismPositionerBuilder
Represents a
SubmechanismPositioner builder To create a new instance of this class, use SubmechanismPositionerCollection.createPositionerBuilder(nxopen.motion.SubmechanismPositioner) Created in NX12.0.0 |
SubmechanismPositionerCollection
Represents a collection of Submechanmism Positioner objects
To obtain an instance of this class, refer to MotionManager Created in NX12.0.0 |
TextBasedElement
Represents a
TextBasedElement . |
TextBasedElementBuilder
Represents a
TextBasedElementBuilder builder To create a new instance of this class, use TextBasedElementCollection.createTextBasedElementBuilder(nxopen.motion.TextBasedElement) Created in NX12.0.0 |
TextBasedElementBuilder.TypeChoices
the text based element type - multiple values
|
TextBasedElementCollection
Represents a collection of Text Based Element objects
To obtain an instance of this class, refer to MotionManager Created in NX12.0.0 |
Tire
Tire Motion element. |
TireBuilder
Represents a
Tire builder To create a new instance of this class, use TireCollection.createTireBuilder(nxopen.motion.Tire) Default values. |
TireBuilder.Type
the Tire type.
|
TireCollection
Represents a collection of motion tire elements
To obtain an instance of this class, refer to MotionManager Created in NX11.0.0 |
TireProperty
Tire Property element.
|
TirePropertyAdvancedParameters
Represents a TirePropertyAdvancedParameters builder .
|
TirePropertyAdvancedParameters.ContactType
The block type can be Function when a spline curve is used or
Profile when a profile is used.
|
TirePropertyAdvancedParameters.FrictType
The block type can be Function when a spline curve is used or
Profile when a profile is used.
|
TirePropertyAdvancedParameters.RollingType
the rolling radius type.
|
TirePropertyAdvancedParameters.SurfType
the type of surface interaction calculations used.
|
TirePropertyBasic
Basic Tire Property element. |
TirePropertyBasicBuilder
Represents a builder for a
TirePropertyBasic To create a new instance of this class, use TirePropertyBasicCollection.createTirePropertyBasicBuilder(nxopen.motion.TirePropertyBasic) Default values. |
TirePropertyBasicCollection
Represents a collection of
TirePropertyBasic elements To obtain an instance of this class, refer to MotionManager Created in NX11.0.0 |
TirePropertyBasicParameters
Represents a TirePropertyBasicParameters builder .
|
TirePropertyBasicParameters.CorneringType
A constant will be used for the Cornering Stiffness when CorneringType is 'Cornering'.
|
TirePropertyBuilder
Represents a Builder base class for Tire Properties
This is an abstract class, and cannot be created. |
TirePropertyCd
CDTIRE Tire Property
This is an object that contains parameters needed for the CDTIRE Tire model
To create or edit an instance of this class, use TirePropertyCdBuilder Created in NX11.0.0 |
TirePropertyCdBuilder
Represents a
TirePropertyCd builder To create a new instance of this class, use TirePropertyCdCollection.createTirePropertyCdBuilder(nxopen.motion.TirePropertyCd) Default values. |
TirePropertyCdBuilder.AmbientTempType
The Ambient Temp type.
|
TirePropertyCdBuilder.InflationPressureType
The Inflation Pressure type.
|
TirePropertyCdBuilder.ModelType
The Model type.
|
TirePropertyCdCollection
Represents a collection of Motion CDTire Tire Property elements
To obtain an instance of this class, refer to MotionManager Created in NX11.0.0 |
TirePropertyFt
FTire Tire Property element
This is an object that contains parameters needed for the FTire Tire model
To create or edit an instance of this class, use TirePropertyFtBuilder Created in NX11.0.0 |
TirePropertyFtBuilder
Represents a Builder for Motion Ftire Tire Property
To create a new instance of this class, use TirePropertyFtCollection.createTirePropertyFtBuilder(nxopen.motion.TirePropertyFt) Default values. |
TirePropertyFtCollection
Represents a collection of Motion FTire Tire Property elements
To obtain an instance of this class, refer to MotionManager Created in NX11.0.0 |
TirePropertyHighOrderParameters
Represents a Tire Property builder for the High Order parameters used in Motorcycle and Basic properties.
|
TirePropertyHighOrderParameters.UnloadingVertStiffType
The block type can be Function when a spline curve is used or
Profile when a profile is used.
|
TirePropertyMotorcycle
Motorcycle Tire Property element. |
TirePropertyMotorcycleBuilder
Represents a TirePropertyMotorcycleBuilder builder
To create a new instance of this class, use TirePropertyMotorcycleCollection.createTirePropertyMotorcycleBuilder(nxopen.motion.TirePropertyMotorcycle) Default values. |
TirePropertyMotorcycleCollection
Represents a collection of Motion Motorcycle Tire Property elements
To obtain an instance of this class, refer to MotionManager Created in NX11.0.0 |
TirePropertyNonInertial
NonInertial Tire Property element. |
TirePropertyNonInertialBuilder
Represents a builder for a Non-inertial Tire Property
To create a new instance of this class, use TirePropertyNonInertialCollection.createTirePropertyNonInertialBuilder(nxopen.motion.TirePropertyNonInertial) Default values. |
TirePropertyNonInertialCollection
Represents a collection of Motion Non-inertial Tire Property elements
To obtain an instance of this class, refer to MotionManager Created in NX11.0.0 |
TirePropertyTno
TNO Tire Property element
This is an object that contains parameters needed for the TNO Tire model
To create or edit an instance of this class, use TirePropertyTnoBuilder Created in NX11.0.0 |
TirePropertyTnoBuilder
Represents a Builder for Motion TNO Tire Property.
|
TirePropertyTnoBuilder.ContactMethodType
The Contact Method type.
|
TirePropertyTnoBuilder.DynamicsType
The Dynamics type.
|
TirePropertyTnoBuilder.IswitchDefinitionType
The Iswitch Definition type.
|
TirePropertyTnoBuilder.SlipForcesType
The Slip Forces type.
|
TirePropertyTnoBuilder.TireSideType
The Tire Side type.
|
TirePropertyTnoBuilder.TrackSideType
The Track Side type.
|
TirePropertyTnoCollection
Represents a collection of Motion Tno Tire Property elements
To obtain an instance of this class, refer to MotionManager Created in NX11.0.0 |
UserDefinedSection
Represents a user defined section function
To create or edit an instance of this class, use UserDefinedSectionBuilder Created in NX12.0.0 |
UserDefinedSectionBuilder
Represents a
UserDefinedSectionBuilder . |
VectorForce
Represents a vector force
To create or edit an instance of this class, use VectorForceBuilder Created in NX5.0.0 |
VectorForceBuilder
Represents a
VectorForceBuilder
To create a new instance of this class, use VectorForceCollection.createVectorForceBuilder(nxopen.motion.VectorForce) Created in NX5.0.0 |
VectorForceCollection
Represents a collection of vector force objects
To obtain an instance of this class, refer to MotionManager Created in NX5.0.0 |
VectorTorque
Represents a vector torque
To create or edit an instance of this class, use VectorTorqueBuilder Created in NX5.0.0 |
VectorTorqueBuilder
Represents a
VectorTorqueBuilder
To create a new instance of this class, use VectorTorqueCollection.createVectorTorqueBuilder(nxopen.motion.VectorTorque) Created in NX5.0.0 |
VectorTorqueCollection
Represents a collection of vector torque objects
To obtain an instance of this class, refer to MotionManager Created in NX5.0.0 |
VObject
Represents a VObject
.
|
VobjectApplicationType
the application type.
|
VobjectCsysType
Represents the CSYS type
|
Class and Description |
---|
Graph
Represents a graph, only creation is supported
To create or edit an instance of this class, use GraphObjectBuilder Created in NX5.0.0 |
MotionSolution
Represents a solution
To create or edit an instance of this class, use MotionSolutionBuilder Created in NX5.0.0 |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.