Package | Description |
---|---|
nxopen.motion |
Provides classes and interfaces for Motion Simulation.
|
Modifier and Type | Method and Description |
---|---|
ControlInputPortBuilder |
ControlInputBuilder.createControlInputPortBuilder()
Creates a new control input port item and adds to the PortsList.
|
ControlInputPortBuilder |
ControlInputPortBuilderList.findItem(int index)
Returns the object at the input index.
|
ControlInputPortBuilder[] |
ControlInputPortBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
ControlInputPortBuilderList.append(ControlInputPortBuilder object)
Appends an object to the list
License requirements: None. |
void |
ControlInputPortBuilderList.append(ControlInputPortBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
ControlInputPortBuilderList.erase(ControlInputPortBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
ControlInputPortBuilderList.erase(ControlInputPortBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
ControlInputPortBuilderList.findIndex(ControlInputPortBuilder obj)
Finds the index where the input object appears.
|
void |
ControlInputPortBuilderList.insert(int location,
ControlInputPortBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
ControlInputPortBuilderList.setContents(ControlInputPortBuilder[] objects)
Sets the contents of the entire list.
|
void |
ControlInputPortBuilderList.swap(ControlInputPortBuilder object1,
ControlInputPortBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.