Package | Description |
---|---|
nxopen.motion |
Provides classes and interfaces for Motion Simulation.
|
Modifier and Type | Field and Description |
---|---|
static PackagingMeasureBuilder.MeasureCondition |
PackagingMeasureBuilder.MeasureCondition.EQUAL_TO
Stop event defined by minimum measurement
equal to threshold (target) value.
|
static PackagingMeasureBuilder.MeasureCondition |
PackagingMeasureBuilder.MeasureCondition.GREATER_THAN
Stop event defined by minimum measurement
greater than threshold value.
|
static PackagingMeasureBuilder.MeasureCondition |
PackagingMeasureBuilder.MeasureCondition.LESS_THAN
Stop event defined by minimum measurement
less than threshold value.
|
Modifier and Type | Method and Description |
---|---|
PackagingMeasureBuilder.MeasureCondition |
PackagingMeasureBuilder.condition()
Returns the measure condition defined at
PackagingMeasureBuilder.MeasureCondition
License requirements: mechanisms ("MECHANISMS") Created in NX4.0.0 |
static PackagingMeasureBuilder.MeasureCondition |
PackagingMeasureBuilder.MeasureCondition.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PackagingMeasureBuilder.MeasureCondition |
PackagingMeasureBuilder.MeasureCondition.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PackagingMeasureBuilder.MeasureCondition[] |
PackagingMeasureBuilder.MeasureCondition.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PackagingMeasureBuilder.setCondition(PackagingMeasureBuilder.MeasureCondition condition)
Sets the measure condition defined at
PackagingMeasureBuilder.MeasureCondition
License requirements: mechanisms ("MECHANISMS") Created in NX4.0.0 |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.