Package | Description |
---|---|
nxopen.motion |
Provides classes and interfaces for Motion Simulation.
|
Modifier and Type | Method and Description |
---|---|
PortVariable |
PortVariableList.findItem(int index)
Returns the object at the input index.
|
PortVariable[] |
PortVariableList.getContents()
Gets the contents of the entire list
License requirements: None. |
PortVariable |
MechatronicsBuilder.getPortVariable(String inputName)
Searches for the watch variable by name in the active group
License requirements: mechanisms ("MECHANISMS") . |
Modifier and Type | Method and Description |
---|---|
void |
PortVariableList.append(PortVariable object)
Appends an object to the list
License requirements: None. |
void |
PortVariableList.append(PortVariable[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
PortVariableList.erase(PortVariable obj)
Erases the object from the list, but does not delete the object.
|
void |
PortVariableList.erase(PortVariable obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
PortVariableList.findIndex(PortVariable obj)
Finds the index where the input object appears.
|
void |
PortVariableList.insert(int location,
PortVariable object)
Inserts an object at the specified location
License requirements: None. |
void |
PortVariableList.setContents(PortVariable[] objects)
Sets the contents of the entire list.
|
void |
PortVariableList.swap(PortVariable object1,
PortVariable object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.