Package | Description |
---|---|
nxopen.motion |
Provides classes and interfaces for Motion Simulation.
|
Modifier and Type | Interface and Description |
---|---|
interface |
AnalyticalContact
Represents an Analytical Contact motion object.
|
interface |
AnalyticalContactProperty
Represents an Analytical Contact Property.
|
interface |
BaseSection
Represents a base section function
To create or edit an instance of this class, use BaseSectionBuilder Created in NX12.0.0 |
interface |
BeamForce
Represents a BeamForce
To create or edit an instance of this class, use BeamForceBuilder Created in NX12.0.0 |
interface |
BodyContact
Represents a
BodyContact
To create or edit an instance of this class, use BodyContactBuilder Created in NX5.0.0 |
interface |
Bushing
Represents a bushing
To create or edit an instance of this class, use BushingBuilder Created in NX6.0.0 |
interface |
Connector
Represents a connector
This is an abstract class, and cannot be created. |
interface |
ControlInput
Represents a Control Input motion object.
|
interface |
ControlOutput
Represents a Control Output motion object.
|
interface |
ControlPort
Represents a motion control port object class.
|
interface |
Coupler
Represents a motion coupler object
This is an abstract class, and cannot be created. |
interface |
CouplerCable
Represents a motion cable object
To create or edit an instance of this class, use CouplerCableBuilder Created in NX6.0.0 |
interface |
CouplerGear
Represents a motion gear object
To create or edit an instance of this class, use CouplerGearBuilder Created in NX6.0.0 |
interface |
CouplerRckpn
Represents a motion rack and pinion object
To create or edit an instance of this class, use CouplerRckpnBuilder Created in NX6.0.0 |
interface |
CurveContact
Represents a
CurveContact
To create or edit an instance of this class, use CurveContactBuilder Created in NX5.0.0 |
interface |
CurveOnCurve
Represents a curve on curve
To create or edit an instance of this class, use CurveOnCurveBuilder Created in NX6.0.0 |
interface |
Damper
Represents a damper
To create or edit an instance of this class, use DamperBuilder Created in NX6.0.0 |
interface |
FlexBody
Represents the Motion FlexBody class.It must be associated
with a Motion Link.
|
interface |
GeneralCoupler
Represents motion 2-3 joint coupler
To create or edit an instance of this class, use GeneralCouplerBuilder Created in NX7.5.0 |
interface |
Joint
Represents a motion joint object
To create or edit an instance of this class, use JointBuilder Created in NX5.0.0 |
interface |
JointDriver
Represents a joint driver
To create or edit an instance of this class, use JointDriverBuilder Created in NX5.0.0 |
interface |
Link
Represents the Motion Link class.
|
interface |
LinkCoupler
Represents a
LinkCoupler To create or edit an instance of this class, use LinkCouplerBuilder Created in NX12.0.0 |
interface |
LinkDriver
Represents a Link Driver
To create or edit an instance of this class, use LinkDriverBuilder Created in NX11.0.0 |
interface |
LoadTransfer
Represents a Motion Load Transfer class
To create or edit an instance of this class, use LoadTransferBuilder Created in NX9.0.0 |
interface |
Mechatronics
Represents a
Mechatronics . |
interface |
MotionSensor
Represents a motion sensor
To create or edit an instance of this class, use MotionSensorBuilder Created in NX6.0.0 |
interface |
Motor
Represents a motion motor base object class
This is an abstract class, and cannot be created. |
interface |
PMDCMotor
Represents a motion pmdc motor object
To create or edit an instance of this class, use PMDCMotorBuilder Created in NX6.0.0 |
interface |
PointOnCurve
Represents a point on curve
To create or edit an instance of this class, use PointOnCurveBuilder Created in NX6.0.0 |
interface |
PointOnSurface
Represents a point on surface motion object
To create or edit an instance of this class, use PointOnSurfaceBuilder Created in NX6.0.0 |
interface |
Road
|
interface |
ScalarForce
Represents the Motion ScalarForce class.
|
interface |
ScalarTorque
Represents the Motion ScalarTorque class.
|
interface |
SplineBeam
Represents a SplineBeam
To create or edit an instance of this class, use SplineBeamBuilder Created in NX12.0.0 |
interface |
SplineBeamProperty
Represents a SplineBeam Property
To create or edit an instance of this class, use SplineBeamPropertyBuilder Created in NX12.0.0 |
interface |
Spring
Represents a spring
To create or edit an instance of this class, use SpringBuilder Created in NX6.0.0 |
interface |
StandardSection
Represents a standard beam section
To create or edit an instance of this class, use StandardSectionBuilder Created in NX12.0.0 |
interface |
TextBasedElement
Represents a
TextBasedElement . |
interface |
Tire
Tire Motion element. |
interface |
TireProperty
Tire Property element.
|
interface |
TirePropertyBasic
Basic Tire Property element. |
interface |
TirePropertyCd
CDTIRE Tire Property
This is an object that contains parameters needed for the CDTIRE Tire model
To create or edit an instance of this class, use TirePropertyCdBuilder Created in NX11.0.0 |
interface |
TirePropertyFt
FTire Tire Property element
This is an object that contains parameters needed for the FTire Tire model
To create or edit an instance of this class, use TirePropertyFtBuilder Created in NX11.0.0 |
interface |
TirePropertyMotorcycle
Motorcycle Tire Property element. |
interface |
TirePropertyNonInertial
NonInertial Tire Property element. |
interface |
TirePropertyTno
TNO Tire Property element
This is an object that contains parameters needed for the TNO Tire model
To create or edit an instance of this class, use TirePropertyTnoBuilder Created in NX11.0.0 |
interface |
UserDefinedSection
Represents a user defined section function
To create or edit an instance of this class, use UserDefinedSectionBuilder Created in NX12.0.0 |
interface |
VectorForce
Represents a vector force
To create or edit an instance of this class, use VectorForceBuilder Created in NX5.0.0 |
interface |
VectorTorque
Represents a vector torque
To create or edit an instance of this class, use VectorTorqueBuilder Created in NX5.0.0 |
Modifier and Type | Method and Description |
---|---|
MotionObject |
AdoptionPair.adoption()
Returns an adoption object
License requirements: mechanisms ("MECHANISMS") . |
Modifier and Type | Method and Description |
---|---|
AdoptionPair |
AdoptionPairCollection.createPair(NXObject source,
MotionObject adoption)
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.