Package | Description |
---|---|
nxopen.motion |
Provides classes and interfaces for Motion Simulation.
|
Modifier and Type | Interface and Description |
---|---|
interface |
ConfigurationFloatParameter
Represents a
ConfigurationFloatParameter . |
interface |
ConfigurationIntegerParameter
Represents a
ConfigurationIntegerParameter . |
interface |
ConfigurationTextParameter
Represents a
ConfigurationTextParameter . |
Modifier and Type | Method and Description |
---|---|
ConfigurationParameter |
ConfigurationParameterList.findItem(int index)
Returns the object at the input index.
|
ConfigurationParameter |
MechatronicsBuilder.getConfigurationParameter(String inputName)
Searches for the watch parameter by name in the active group
License requirements: mechanisms ("MECHANISMS") . |
ConfigurationParameter[] |
ConfigurationParameterList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
ConfigurationParameterList.append(ConfigurationParameter object)
Appends an object to the list
License requirements: None. |
void |
ConfigurationParameterList.append(ConfigurationParameter[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
ConfigurationParameterList.erase(ConfigurationParameter obj)
Erases the object from the list, but does not delete the object.
|
void |
ConfigurationParameterList.erase(ConfigurationParameter obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
ConfigurationParameterList.findIndex(ConfigurationParameter obj)
Finds the index where the input object appears.
|
void |
ConfigurationParameterList.insert(int location,
ConfigurationParameter object)
Inserts an object at the specified location
License requirements: None. |
void |
ConfigurationParameterList.setContents(ConfigurationParameter[] objects)
Sets the contents of the entire list.
|
void |
ConfigurationParameterList.swap(ConfigurationParameter object1,
ConfigurationParameter object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.