Package | Description |
---|---|
nxopen.motion |
Provides classes and interfaces for Motion Simulation.
|
Modifier and Type | Field and Description |
---|---|
static GeneralCouplerBuilder.AttachmentType |
GeneralCouplerBuilder.AttachmentType.THREE
three-joint coupler type
|
static GeneralCouplerBuilder.AttachmentType |
GeneralCouplerBuilder.AttachmentType.TWO
two-joint coupler type
|
Modifier and Type | Method and Description |
---|---|
GeneralCouplerBuilder.AttachmentType |
GeneralCouplerBuilder.attachment()
Returns the attachment type
License requirements: None. |
static GeneralCouplerBuilder.AttachmentType |
GeneralCouplerBuilder.AttachmentType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static GeneralCouplerBuilder.AttachmentType |
GeneralCouplerBuilder.AttachmentType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static GeneralCouplerBuilder.AttachmentType[] |
GeneralCouplerBuilder.AttachmentType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
GeneralCouplerBuilder.setAttachment(GeneralCouplerBuilder.AttachmentType attachment)
License requirements: mechanisms ("MECHANISMS") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.