Package | Description |
---|---|
nxopen.motion |
Provides classes and interfaces for Motion Simulation.
|
Modifier and Type | Method and Description |
---|---|
OutputPortAssociation |
OutputPortAssociationList.findItem(int index)
Returns the object at the input index.
|
OutputPortAssociation[] |
OutputPortAssociationList.getContents()
Gets the contents of the entire list
License requirements: None. |
OutputPortAssociation |
MechatronicsBuilder.getOutput(String inputName)
Retrieves an output port association from its name
License requirements: mechanisms ("MECHANISMS") . |
OutputPortAssociation |
MechatronicsBuilder.newOutputListItem()
Creates a new output list item including expressions
License requirements: mechanisms ("MECHANISMS") . |
Modifier and Type | Method and Description |
---|---|
void |
OutputPortAssociationList.append(OutputPortAssociation object)
Appends an object to the list
License requirements: None. |
void |
OutputPortAssociationList.append(OutputPortAssociation[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
OutputPortAssociationList.erase(OutputPortAssociation obj)
Erases the object from the list, but does not delete the object.
|
void |
OutputPortAssociationList.erase(OutputPortAssociation obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
OutputPortAssociationList.findIndex(OutputPortAssociation obj)
Finds the index where the input object appears.
|
void |
OutputPortAssociationList.insert(int location,
OutputPortAssociation object)
Inserts an object at the specified location
License requirements: None. |
void |
OutputPortAssociationList.setContents(OutputPortAssociation[] objects)
Sets the contents of the entire list.
|
void |
OutputPortAssociationList.swap(OutputPortAssociation object1,
OutputPortAssociation object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.