Package | Description |
---|---|
nxopen.motion |
Provides classes and interfaces for Motion Simulation.
|
Modifier and Type | Interface and Description |
---|---|
interface |
AnalyticalContact
Represents an Analytical Contact motion object.
|
interface |
BeamForce
Represents a BeamForce
To create or edit an instance of this class, use BeamForceBuilder Created in NX12.0.0 |
interface |
BodyContact
Represents a
BodyContact
To create or edit an instance of this class, use BodyContactBuilder Created in NX5.0.0 |
interface |
Bushing
Represents a bushing
To create or edit an instance of this class, use BushingBuilder Created in NX6.0.0 |
interface |
ControlOutput
Represents a Control Output motion object.
|
interface |
ControlPort
Represents a motion control port object class.
|
interface |
CurveContact
Represents a
CurveContact
To create or edit an instance of this class, use CurveContactBuilder Created in NX5.0.0 |
interface |
CurveOnCurve
Represents a curve on curve
To create or edit an instance of this class, use CurveOnCurveBuilder Created in NX6.0.0 |
interface |
Damper
Represents a damper
To create or edit an instance of this class, use DamperBuilder Created in NX6.0.0 |
interface |
FlexBody
Represents the Motion FlexBody class.It must be associated
with a Motion Link.
|
interface |
GeneralCoupler
Represents motion 2-3 joint coupler
To create or edit an instance of this class, use GeneralCouplerBuilder Created in NX7.5.0 |
interface |
Joint
Represents a motion joint object
To create or edit an instance of this class, use JointBuilder Created in NX5.0.0 |
interface |
Link
Represents the Motion Link class.
|
interface |
LinkCoupler
Represents a
LinkCoupler To create or edit an instance of this class, use LinkCouplerBuilder Created in NX12.0.0 |
interface |
LinkDriver
Represents a Link Driver
To create or edit an instance of this class, use LinkDriverBuilder Created in NX11.0.0 |
interface |
Marker
Represents the Motion Marker class.
|
interface |
MotionFunction
Represents a Motion Function Object
To create or edit an instance of this class, use FunctionBuilder Created in NX11.0.0 |
interface |
MotionSensor
Represents a motion sensor
To create or edit an instance of this class, use MotionSensorBuilder Created in NX6.0.0 |
interface |
PackagingMeasure
This class represents a Packaging Measure object.
|
interface |
PlantInput
Represents a Plant Input motion object
To create or edit an instance of this class, use PlantInputBuilder Created in NX6.0.0 |
interface |
PlantOutput
Represents a Plant Output motion object
To create or edit an instance of this class, use PlantOutputBuilder Created in NX6.0.0 |
interface |
PointOnCurve
Represents a point on curve
To create or edit an instance of this class, use PointOnCurveBuilder Created in NX6.0.0 |
interface |
PointOnSurface
Represents a point on surface motion object
To create or edit an instance of this class, use PointOnSurfaceBuilder Created in NX6.0.0 |
interface |
ScalarForce
Represents the Motion ScalarForce class.
|
interface |
ScalarTorque
Represents the Motion ScalarTorque class.
|
interface |
SplineBeam
Represents a SplineBeam
To create or edit an instance of this class, use SplineBeamBuilder Created in NX12.0.0 |
interface |
Spring
Represents a spring
To create or edit an instance of this class, use SpringBuilder Created in NX6.0.0 |
interface |
Tire
Tire Motion element. |
interface |
VectorForce
Represents a vector force
To create or edit an instance of this class, use VectorForceBuilder Created in NX5.0.0 |
interface |
VectorTorque
Represents a vector torque
To create or edit an instance of this class, use VectorTorqueBuilder Created in NX5.0.0 |
Modifier and Type | Method and Description |
---|---|
IGraphSource |
GraphObjectBuilder.referenceObject()
Returns the reference object of graph object
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
GraphObjectBuilder.setReferenceObject(IGraphSource referObject)
License requirements: mechanisms ("MECHANISMS") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.