Package | Description |
---|---|
nxopen.motion |
Provides classes and interfaces for Motion Simulation.
|
Modifier and Type | Interface and Description |
---|---|
interface |
StandardSection
Represents a standard beam section
To create or edit an instance of this class, use StandardSectionBuilder Created in NX12.0.0 |
interface |
UserDefinedSection
Represents a user defined section function
To create or edit an instance of this class, use UserDefinedSectionBuilder Created in NX12.0.0 |
Modifier and Type | Field and Description |
---|---|
BaseSection |
SelectBaseSection.ValueData.selection
selected object
|
BaseSection |
SelectBaseSection.ValueWithCaeSetObjectInfoData.selection
selected object
|
BaseSection |
SelectBaseSection.ValueWithSnapData.selection1
first selected object
|
BaseSection |
SelectBaseSection.ValueWithSnapData.selection2
second selected object
|
Modifier and Type | Method and Description |
---|---|
BaseSection |
BaseSectionCollection.findObject(String name)
Finds the
BaseSection with the given name. |
BaseSection |
SelectBaseSection.value()
Returns the object being selected
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
SelectBaseSection.setValue(BaseSection selection)
Sets the object being selected
License requirements: None. |
void |
SelectBaseSection.setValue(BaseSection selection,
View view,
Point3d point)
The object being selected with the object's view and object's point
License requirements: None. |
void |
SelectBaseSection.setValueWithCaeSetObjectInfo(BaseSection selection,
CaeObjectType.CaeSubType caeSubType,
int caeSubId)
Deprecated.
Deprecated in NX10.0.0. Use other versions of
SelectObject.setValue(nxopen.TaggedObject) .
|
void |
SelectBaseSection.setValueWithSnap(InferSnapType.SnapType snapType,
BaseSection selection1,
View view1,
Point3d point1,
BaseSection selection2,
View view2,
Point3d point2)
The object being selected with the objects view and objects point and snap information.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.