Package | Description |
---|---|
nxopen.motion |
Provides classes and interfaces for Motion Simulation.
|
Modifier and Type | Method and Description |
---|---|
SegmentBuilder |
RoadBuilder.createSegmentBuilder()
Creates a new segment builder for the road object of type path
License requirements: mechanisms ("MECHANISMS") . |
SegmentBuilder |
SegmentBuilderList.findItem(int index)
Returns the object at the input index.
|
SegmentBuilder[] |
SegmentBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
SegmentBuilder |
RoadBuilder.getSegmentBuilder(int segmentBuilderIndex)
Get a specific segment builder from the list
License requirements: mechanisms ("MECHANISMS") . |
Modifier and Type | Method and Description |
---|---|
void |
SegmentBuilderList.append(SegmentBuilder object)
Appends an object to the list
License requirements: None. |
void |
SegmentBuilderList.append(SegmentBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
SegmentBuilderList.erase(SegmentBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
SegmentBuilderList.erase(SegmentBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
SegmentBuilderList.findIndex(SegmentBuilder obj)
Finds the index where the input object appears.
|
void |
SegmentBuilderList.insert(int location,
SegmentBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
RoadBuilder.removeSegmentBuilder(SegmentBuilder segment)
Remove a segment
License requirements: mechanisms ("MECHANISMS") . |
void |
SegmentBuilderList.setContents(SegmentBuilder[] objects)
Sets the contents of the entire list.
|
void |
SegmentBuilderList.swap(SegmentBuilder object1,
SegmentBuilder object2)
Exchanges the position of two objects inside the list.
|
void |
RoadBuilder.swapSegment(SegmentBuilder firstSegment,
SegmentBuilder secondSegment)
Swap two segments
License requirements: mechanisms ("MECHANISMS") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.