Package | Description |
---|---|
nxopen.motion |
Provides classes and interfaces for Motion Simulation.
|
Modifier and Type | Field and Description |
---|---|
static ConnectorBuilder.AttachmentType |
ConnectorBuilder.AttachmentType.LINK
connector is attacted to links
|
static ConnectorBuilder.AttachmentType |
ConnectorBuilder.AttachmentType.REVOLUTE_JOINT
connector is attacted to revolute joint
|
static ConnectorBuilder.AttachmentType |
ConnectorBuilder.AttachmentType.SLIDER_JOINT
connector is attacted to slider joint
|
Modifier and Type | Method and Description |
---|---|
ConnectorBuilder.AttachmentType |
ConnectorBuilder.attachment()
Returns the attachment type
License requirements: None. |
static ConnectorBuilder.AttachmentType |
ConnectorBuilder.AttachmentType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ConnectorBuilder.AttachmentType |
ConnectorBuilder.AttachmentType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ConnectorBuilder.AttachmentType[] |
ConnectorBuilder.AttachmentType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ConnectorBuilder.setAttachment(ConnectorBuilder.AttachmentType attachment)
License requirements: mechanisms ("MECHANISMS") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.