Package | Description |
---|---|
nxopen.motion |
Provides classes and interfaces for Motion Simulation.
|
Modifier and Type | Field and Description |
---|---|
static FlexBodyBuilder.UnitSystemType |
FlexBodyBuilder.UnitSystemType.CENTIMETER_CENTINEWTON
(cN)(cm)(kg)
|
static FlexBodyBuilder.UnitSystemType |
FlexBodyBuilder.UnitSystemType.FOOT_POUNDAL
(poundal)(ft)(lbm)
|
static FlexBodyBuilder.UnitSystemType |
FlexBodyBuilder.UnitSystemType.FOOT_POUNDAL_F
(lbf)(ft)(slug)
|
static FlexBodyBuilder.UnitSystemType |
FlexBodyBuilder.UnitSystemType.INCH_POUND_F
(lbf)(in)(lbf-s^2/in)
|
static FlexBodyBuilder.UnitSystemType |
FlexBodyBuilder.UnitSystemType.INFERED
unit system of file
|
static FlexBodyBuilder.UnitSystemType |
FlexBodyBuilder.UnitSystemType.METER_KILOGRAM_F
(kgf)(m)(kgf-s^2/m)
|
static FlexBodyBuilder.UnitSystemType |
FlexBodyBuilder.UnitSystemType.METER_NEWTON
(N)(m)(kg)
|
static FlexBodyBuilder.UnitSystemType |
FlexBodyBuilder.UnitSystemType.MILLIMETER_KILOGRAM_F
(kgf)(mm)(kgf-s^2/mm)
|
static FlexBodyBuilder.UnitSystemType |
FlexBodyBuilder.UnitSystemType.MILLIMETER_MILLINEWTON
(mN)(mm)(kg)
|
static FlexBodyBuilder.UnitSystemType |
FlexBodyBuilder.UnitSystemType.MILLIMETER_NEWTON
(N)(mm)(tonne)
|
Modifier and Type | Method and Description |
---|---|
FlexBodyBuilder.UnitSystemType |
FlexBodyBuilder.unitSystem()
Returns the unit system ID
License requirements: None. |
static FlexBodyBuilder.UnitSystemType |
FlexBodyBuilder.UnitSystemType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FlexBodyBuilder.UnitSystemType |
FlexBodyBuilder.UnitSystemType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FlexBodyBuilder.UnitSystemType[] |
FlexBodyBuilder.UnitSystemType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
FlexBodyBuilder.setUnitSystem(FlexBodyBuilder.UnitSystemType unitSystemID)
License requirements: mechanisms ("MECHANISMS") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.