Package | Description |
---|---|
nxopen.motion |
Provides classes and interfaces for Motion Simulation.
|
Modifier and Type | Field and Description |
---|---|
static MotionSolutionBuilder.AnalysisTypes |
MotionSolutionBuilder.AnalysisTypes.CONTROL |
static MotionSolutionBuilder.AnalysisTypes |
MotionSolutionBuilder.AnalysisTypes.DYNAMIC
Dynamic or Kinematic analysis
|
static MotionSolutionBuilder.AnalysisTypes |
MotionSolutionBuilder.AnalysisTypes.STATIC
Static analysis
|
Modifier and Type | Method and Description |
---|---|
MotionSolutionBuilder.AnalysisTypes |
MotionSolutionBuilder.analysisType()
Returns the analysis type
License requirements: None. |
static MotionSolutionBuilder.AnalysisTypes |
MotionSolutionBuilder.AnalysisTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MotionSolutionBuilder.AnalysisTypes |
MotionSolutionBuilder.AnalysisTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MotionSolutionBuilder.AnalysisTypes[] |
MotionSolutionBuilder.AnalysisTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
MotionSolutionBuilder.setAnalysisType(MotionSolutionBuilder.AnalysisTypes analysisType)
License requirements: mechanisms ("MECHANISMS") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.