Package | Description |
---|---|
nxopen.motion |
Provides classes and interfaces for Motion Simulation.
|
Modifier and Type | Field and Description |
---|---|
static MotionSolutionBuilder.SolutionTypes |
MotionSolutionBuilder.SolutionTypes.ARTICULATION
Articulation run
|
static MotionSolutionBuilder.SolutionTypes |
MotionSolutionBuilder.SolutionTypes.FLEXBODY
Flexible Body Dynamics run
|
static MotionSolutionBuilder.SolutionTypes |
MotionSolutionBuilder.SolutionTypes.NORMAL
Normal run
|
static MotionSolutionBuilder.SolutionTypes |
MotionSolutionBuilder.SolutionTypes.SPREADSHEET
Spreadsheet run
|
Modifier and Type | Method and Description |
---|---|
MotionSolutionBuilder.SolutionTypes |
MotionSolutionBuilder.solutionType()
Returns the solution type
License requirements: None. |
static MotionSolutionBuilder.SolutionTypes |
MotionSolutionBuilder.SolutionTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MotionSolutionBuilder.SolutionTypes |
MotionSolutionBuilder.SolutionTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MotionSolutionBuilder.SolutionTypes[] |
MotionSolutionBuilder.SolutionTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
MotionSolutionBuilder.setSolutionType(MotionSolutionBuilder.SolutionTypes solutionType)
License requirements: mechanisms ("MECHANISMS") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.